Hello Clock and Timing Experts,
I need to support two VCXO frequencies using the AD9528. Since the PLL1 Input Receiver Control Register let me select single ended VCXO clock from either negative or positive VCXO_IN pins, I wonder if I can use this to multiplex the two VCXOs.
Figure 25 in the datasheet shows configuration with one single ended CMOS clock, where one of the VCXO_IN inputs is decoupled to GND via a 0.1uF capacitor instead of having this pin floating.
I wonder if my trick would work and I can save PCB space for an additional clock multiplexer?