ADF4002 parameters

Hello

          Customer use 10MHz reference clock to Ref of ADF4002. They would like to get output frequency is 128.88MHz. We help setting these parameters as attached. Has any problem or risk of ADF4002 setting for 128.88MHz ?  

          Another question, if use fractional PLL, has any suggest solution for it ? Thank you.  

https://drive.google.com/file/d/10U7Ze_zawiivSqxNXEBgL6NZaD-N8cK_/view?usp=sharing 

BR

Patrick



Fractional PLL
[edited by: patrickchen@morrihan.com at 2:16 PM (GMT -5) on 5 Feb 2021]
Parents
  • +1
    •  Analog Employees 
    on Feb 10, 2021 10:51 PM

    The ADF4002 is an integer PLL.  Did they want a fractional PLL.  Here is the list the ADIsimPLL came up with for fractional options.

    The decision from here will be based on how good of phase noise vs power dissipation performance they desire vs cost.  Did you have any phase noise rqmts?

  • Hello 

           If customer use ADF4150 for 122.88MHz output frequency to replace ADF4002,is it a suitable fractional PLL solution ?

           Per below schematics, 122.88MHz comes from RF INA for clock output and not comes from RD OUTA/RF OUTB with 122.88MHz VCO.

            Is it ok if not through RF OUTA/ RF OUTB  ? Thank you. 

    BR

    Patrick 

  • Hello Alex

               Has any suggestion for above? Thank you. 

    BR

    Patrick

  • +1
    •  Analog Employees 
    on Mar 9, 2021 5:04 PM in reply to patrickchen@morrihan.com

    Hi Patrick,

    I think even with a square wave VCO it will be difficult to get enough slew rate to get the ADF4150 to work with RFIN = 122.88MHz. 

    As mentioned before I think it would be better to find a VCO which could cover 983.04MHz or 1966.08MHz range and use the output divider. If you are at these frequencies then a square wave VCO is not required. In fact a sine wave VCO would probably be better for designing matching network purposes.

    If an integer N PLL will be acceptable, the ADF4002 would be a reasonable choice. You could get 122.88MHz by using a 10MHz reference and a PFD frequency of 640kHz as an example. Are multiple channels required, or just one frequency? With integer N PLLs you will only be able to get channel spacing equal to the PFD frequency. If you are just trying to get one frequency, then integer N PLL is normally a better choice. Simulating with ADIsimPLL is best to make sure the design will meet your phase noise requirements.


    Note, the ADF4002 also has the same issues with interfacing with CMOS RF inputs as noted previously with the ADF4150. So please beware that that VCO you have proposed will also some require way to reduce the VCO signal level. But the ADF4002 as a lower min RF frequency so slew rate will be less of a concern than the ADF4150.

    https://ez.analog.com/rf/f/q-a/73844/adf4001---interfacing-cmos-vcxo-to-rfin


    Regards,

    Alex

  • Hello Alex

        Customer just require one frequency of 122.88MHz so ADF4002 is also suitable for requirement , right? 

         Another question, I know if use VCO (983.04MHz or 1966.08MHz range) and use the output divider is better for ADF4150. But the customer board already gerber out PCB. So 122.28MHz is ensured not locked PLL of ADF4150, right? 

         if We need to modify on board.,

    1. choose another VCO ((983.04MHz or 1966.08MHz )

    2. tuning resistor divider to meet  RFIN signal level

    3. Jump wire from RFOUT to connect 122.88MHz by schematics

    Thank you. 

     

  • +1
    •  Analog Employees 
    on Mar 12, 2021 4:16 PM in reply to patrickchen@morrihan.com

    Hi Patrick,

    If you wanted to go ahead with that board, this might work:

    Find a VCO covering 983.04MHz or 1966.08MHz range and will fit in the footprint and same pinout as the 9x14mm you have. Some VCOs have larger or smaller cases but the pads may still align. 

    Disconnect C7642, R476, R3404. Then populate these three footprints with 3 resistors in a Pi attenuation network, calculate resistor values to meet RFIN signal level. (Might not be required depending on VCO Pout)

    Remove C7641. 

    Remove R91372, somehow connect RFOUT+ to the 2 pin of C7641.

    The biggest issue I see with this is that the signal integrity of RFOUT+ will be poor by running a wire over, it really needs 50Ohm line. But it might be okay to see if PLL is locked or not.

    Also, loop filter will need redesigned if you are changing VCO! Its likely that ADIsimPLL will have the VCO model, if not then just use custom VCO model in simPLL and enter kVCO and input capacitance from the VCO's datasheet. You will need a VCO with a tuning range between 0.5V and 5V since I am assuming this board has a passive loop filter.

    Regards,

    Alex

  • Hello Alex

                 We modify customer board now. If we choose below 983.04MHz, is it ok? If we modify depend on above your suggestion, how to confirm PLL is locked while no any SPI configuration? Are correct for below pin status while PLL locked? Thank you.  

    LD Pin(External Pull High): High

    MUXOUT: High

    CPOUT: VP/2=3.3V/2=1.5V

    RFOUT: 0.8Vpkpk ( while RFIN 0.8V pkpk) 

    983.04MHz VCO

    https://www.mouser.com/datasheet/2/368/Si550-1100864.pdf 

    BR

    Patrick

Reply Children