ad9542 IEEE 1588 sync

Hello

           Customer FPGA will get IEEE 1588 Timestamps  then sync AD9542. How to sync IEEE 1588 with AD9542? 

           Customer have two questions.

1. Customer get IEEE 1588 Timestamps   then use SPI to tuning output clock for synchronization. if they input syncE(156,25MHz) to AD9542 for reference clock and enter DPLL, it it ok for IEEE 1588 synchronization? or they need close DPLL to let AD9542 at open loop situation the use SPI tuning output clock for  synchronization? Is it normal? 

2. PLL1 setting to syncE,use REF A as reference input , PLL0 setting to 1588, If PLL1 use snycE for synchronization,  is it possible to enter PLL0 for reference clock?  

BR

Patrick

  • +1
    •  Analog Employees 
    on Jan 5, 2021 9:09 PM 1 month ago

    Hi Patrick,

    This is not a simple issue and will probably require more interaction with your customer.  I will attempt to answer your questions and also ask for additional information for clarity.  The AD9542 can be used in many different ways.

    1) The customer will need a 1588 Servo that produces frequency adjustments in parts-per-billion (ppb) relative to the AD9542's present output frequency.  We can provide python code written in the style of C to convert the ppb adjustment to the correct SPI/I2C writes for one of the DPLL's free running tuning words (FRTW).  Programming the FRTW should include safeguards to ensure that the frequency step is not too large to cause the DPLL's subsequent APLL to come unlocked.  

    I will attach a diagram that shows one way to configure the AD9542 for SyncE and 1588 Servo's.  The process leverages the AD9542's System Clock Compensation function.  SyncE is used as an input to DPLL0.  The outputs of Ch0 will have the stability of the SyncE source.  Furthermore the SyncE stability provides System Clock Compensation to DPLL1.  DPLL1 is operated in open loop mode.  This means that the output frequency is a function of the FRTW (updated by the 1588 Servo) and the System Clock (compensated by SyncE).  Please see the System Clock Compensation section in the AD9545 datasheet.  (The AD9542 datasheet is being updated to match the AD9545 for common functions.)

    There are other ways to configure the AD9542 that depend on Holdover requirements during the loss of 1588 and/or SyncE.  It is also important to consider what the output clocks (not just the clocks feeding back to the FPGA/ASIC for the 1588 Servo) require.  Please check with your customer to determine the reference for each of the output channels.

    2) I'm not sure I understand your 2nd question.  DPLL1 can have SyncE as its reference.  DPLL0 can be controlled by the 1588 servo as mentioned above.  As I noted above, we can apply System Clock Compensation to DPLL0 based on the stability of DPLL1.  This will limit DPLL0's wander between SPI/I2C writes match the stability of SyncE.

  • +1
    •  Analog Employees 
    on Jan 5, 2021 10:09 PM 1 month ago in reply to ad9020
  • +1
    •  Analog Employees 
    on Jan 6, 2021 6:40 PM 1 month ago in reply to ad9020

    Patrick, I wanted to mention one additional item.  Your ACE configuration indicates 156.25MHz for the SyncE input.  This is a common frequency for transporting SyncE.  However, it can interact w/ the selected System Clock Xtal Frequency of 52MHz (3 x 52MHz = 156MHz).  We have seen a spur on the outputs at 250kHz offset from the carrier (156.25MHz - 156MHz) in this configuration.  I'd recommend that your customer pick a different frequency for transporting SyncE to the 9542 or change the Xtal frequency of the System Clock.  Either solution resolves the situation.  For instance, a 48MHz Xtal might also produce a spur, but it would be at a 12.25MHz offset from the carrier.  This is an advantage of our AD9545 family of devices that allows flexibility in frequency planning.

  • Hello

               If all output clock used for IEEE1588 related device, both DPLLs should set to open loop and controlled by PTP4L. In this condition, we cannot use any reference input (REFA/REFB) as reference clock, am I right?

               if customer will use 30.72 MHz or 12.8MHz as system clock. if these two frequency is OK?

    BR

    Patrick

  • +1
    •  Analog Employees 
    on Jan 14, 2021 2:14 PM 1 month ago in reply to patrickchen@morrihan.com

    A better configuration is to have one of the DPLL's in open loop and have the other DPLL in cascade mode.  See Cascaded DPLL Configuration section in the AD9545 DS.  This mode creates a Leader/Follower configuration where the Leader DPLL is open loop and controlled by the 1588 Servo updates to the Free Run Tuning Word.  The Follower DPLL uses the feedback of the Leader DPLL as its reference input.  This ensures that both DPLL's track.

    A SyncE (or other stable reference) can still come in on one of the Ref inputs and drive the Aux DPLL.  The Aux DPLL is used for System Clock Compensation of DPLL0/1.  

    System Clock frequencies of 30.72MHz are not recommended because the lower System Clock frequency will degrade phase noise on the outputs.  See the System Clock PLL section of the AD9545 datasheet that recommends System Clock frequencies around 50MHz.  The minimum allowed System Clock is 20MHz.  The System Clock input path needs to have a low phase noise source such as an Xtal for optimum performance.  Furthermore, in Xtal mode the System Clock frequency doubler is used.  The doubler should not be used if the input source is an XO due to concerns about a non-50% input duty cycle.  (This constraint will be noted in an upcoming rev of the AD9545 datasheet.) 

    Use the guidance from my previous response to determine if a spur location associated with a 30.72MHz clock would be a problem.  (156.25MHz - 30.72MHz x 5)