AD9547/8/9 Drift in holdover

How much drift do the AD9547, AD9548, and AD9549 devices exhibit when in holdover mode?

  • +1
    •  Analog Employees 
    on Mar 22, 2011 9:06 PM

    The quick answer is - they add nothing to the drift; they will drift as little or a smuch as the system clock reference source.

    The devices you called out rely on an external system timing source to clock the digital elements of a PLL.  When the devices go into holdover, this system timing reference becomes the time base source and the devices essentially run like a direct digital synthesizer (DDS).  In a DDS, the output frequency has a direct, rational relationship to the system timing clock frequency.  This relationship is established with digital elements that do not drift over time, temperature, or voltage, so there is not even a slight difference between the relative drift that occurs on the system timing source versus that of the output.

  • 0
    •  Analog Employees 
    on May 8, 2019 10:49 AM
    This question has been closed by the EZ team and is assumed answered.