Post Go back to editing

Switch between two TCXOs to feeding ADF4350

Thread Summary

The user needs to design a circuit to switch between two TCXOs for an ADF4350 synthesizer. Analog Devices recommends the ADG619/719/749/779 for single-ended signals and the ADG636/736/787/772 for differential signals. For the specific application of switching between a 26 MHz and a 10 MHz reference clock, the ADG849 or ADG852 is suggested due to their low ON resistance and sufficient bandwidth. The ADG852 has a bandwidth of 100 MHz and an ON resistance of 1.5 Ohms, making it suitable for the application, though jitter performance is not explicitly tested or provided.
AI Generated Content

Dear Sir/Madam:

I need to design ADF4350 synthesizer that can use either one of two TCXOs.  Do you have any switch that can do this job?

The connection is as follows:

                  _______

TCXO1 ----->|Switch |--------->ADF4350

TCXO2 ----->|______|

Thank you

Parents Reply Children
No Data