Post Go back to editing

Switch between two TCXOs to feeding ADF4350

Thread Summary

The user needs to design a circuit to switch between two TCXOs for an ADF4350 synthesizer. Analog Devices recommends the ADG619/719/749/779 for single-ended signals and the ADG636/736/787/772 for differential signals. For the specific application of switching between a 26 MHz and a 10 MHz reference clock, the ADG849 or ADG852 is suggested due to their low ON resistance and sufficient bandwidth. The ADG852 has a bandwidth of 100 MHz and an ON resistance of 1.5 Ohms, making it suitable for the application, though jitter performance is not explicitly tested or provided.
AI Generated Content

Dear Sir/Madam:

I need to design ADF4350 synthesizer that can use either one of two TCXOs.  Do you have any switch that can do this job?

The connection is as follows:

                  _______

TCXO1 ----->|Switch |--------->ADF4350

TCXO2 ----->|______|

Thank you

  • Hi Lotus,

    I assume that the switch shares the supply voltage with the ADF4350(3.3V +/-10%) and the TCXO signals are single ended. If that is the case, you can use any of the following switches: ADG619/719/749/779.

    For diferential TCXO signals the ADG636/736/787/772 can be used.

    Regards,

    FEB

  • Hi, FEB:

    Thank you for your help.  My switch shares the supply voltage with the ADF4350(3.3V +/-10%) and the TCXO signals are single ended.

    Since ADG619/719/749/779 are analog switch, they should not add jitter for the TCXO reference signal, right?

    Thank you in advance.

    Lotus

  • Hi, lotus!

    ADG619/719/749/779  analog switch not add jitter for the TCXO reference signal.

    PSB will be carefully created only.

    Regards!

  • Hi Lotus,

    The analog switch is not jitter free, but if you choose a device with the lowest ON resistance, it will minimize the random jitter due to the noise introduced by the switch resistance. On the other hand, the bandwidth of the switch has to be sufficiently high to pass the signal with minimum distortion to reduce the amount of deterministic jitter introduced by the switch.

    Regards,

    FEB

  • Hi!

    PSB is printed circuit board only .

    Jitter is very-very low, as at passive component (as resistor with equal value ) Don't worry!

  • Hi, FEB:

    Do you have any recommendation which switch to use (with lowest ON resistance) and least jitter.  I have looked at ADG839 with 0.6ohm ON resistance.  But most of parts do not provide jitter information.

    Do you have specs for jitter performance of those switches?

    Thank you in advance.

    Regards

    Lotus

  • Hi, Georgy:

    Thank you for your reply.  What do you mean PSB?  FSB suggested ADG619/719/749/779  analog switch does introduce jitter, I am confused a little bit.  Maybe the jitter is due to the ON resistance uncertainty.

    Regards,

    Lotus

  • Hi Lotus,

    I'm not familiar with TCXOs, but I assume the signal they provide is either a sine or square wave. Would it be possible to share with us some more details about the TCXO signals  such as frequency and rise/fall time(square wave only)?

    Regards,

    FEB

  • Dear FEB:

    The TCXO we use is 26M Hz TCXO with chipper sine wave output.  The part is from NDK.  Please see the attached PDF file.  The chipped sine wave is perfered since it will feed to the ADF4350 synthesize as reference clock.  Squrewave has a lot of harmonics.

    The reason to switch between two TCXOs is that sometimes we need to use external 10M sinewave input instead of this TCXO for synchronization purpose.

    So in this case, we need to switch between this TCXO and external 10M refrence input (typicall Sinewave, from Test equipment).

    Thank you very much.

    Regards,

    Tim

  • Hi Tim,

    Since you want to select between a 10MHz size and the 26MHz TCXO, I would suggest to start by estimating the bandwidth of the 26MHz clipped sine wave from the TXCO and choose a switch with the lowest On resistance that meets the bandwidth criteria.

    The ADG839 has a bandwidth of 25MHz which is less than the fundamental frequency of the TCXO. I would recommend instead the ADG849 which has 38MHz bandwidth with a similar ON resistance or the ADG852 for 100MHz with higher ON resistance of about 1.5 Ohms.

    Regards,

    FEB

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.