Hello. What should be done with the REFB+/- and ZD_IN+/- inputs if they are unused? How about unused OUT+/- pins? Thanks.
Hello. What should be done with the REFB+/- and ZD_IN+/- inputs if they are unused? How about unused OUT+/- pins? Thanks.
Hello,
"Unused input pins" I assume you must be using single-ended CMOS mode. In this case the unused input can be left open since t he circuits will be powered down by SPI register settings.
Output pins can be left open and powered down by SPI register settings.
Regards,
Matt
Matt,
The unused pins I'm asking about are REFB+, REFB-, ZD_IN+, and ZD_IN-. I'm using REFA+ and REFA- as the reference input so REFB+ and REFB- are unused. Also, I am not using the zero-delay inputs ZD_IN+ and ZD_IN-.
Andy
Hi Andy,
The unused input pairs can be left open and there is a register bit to power down the entire receiver or channel in the case of an output.
Thanks,
Matt