fine frequency tunning for high speed ADC clock

Hello Guys

My name is Fernando, I work for the Brazilian National Synchrotron Light Source.

We are designing a fast and broadband four channel digitizer for beam diagnostic pourposes for the next Brazilian light source. The ADC AD9467BCPZ-250 is a natural option for our design, since there is no other 16-bit faster ADC.

So we need to clock these four ADC´s with extremely low jitter signal to get the best SNR possible since the input signal is 500 MHz, so in this case we are using the under sampling technique. The frequency planning is:

We need to lock que clock signal for this 4 adc´s with a external frequency of 500MHz +-1 MHz divide by 800 (any frequency from 623.75 KHz to 626.25 KHz ).  For the ADC´s We need to generate the frequency of:  input lock signal*188, or 248 or 376... besides that we need to have the abilit to generate a fine frequency tunning like: input signal*188+- dozens of Hertz (e.g. 10 or  15 Hz). in a range of 1 Khz or more!

So whats the components from Analog Devices has this ability? how can i configuee these component?

Could give an idea whats the BW of the phase noise I have to considerer to calculate the jitter for these  ADC´s? I guess the most common specification is 12 Khz to 20 Mhz, but is not pratical for data aquisition, i thing the close in phase noise is important...

So guys, thanks in advance!

Fernando Henrique Cardoso

Beam Diagnostics Group (DIG)

Brazilian Synchrotron Light Laboratory (LNLS/CNPEM)

Campinas - Brazil - P.O.Box 6192 - ZIP Code 13083-970

Tel: +55 19 3512-3517 ou 3512-1144//// Cel phone: +55 19 82156023

Fax: +55 19 3512-1004

  • 0
    •  Analog Employees 
    on Mar 6, 2012 8:53 PM

    I think there is a typo in your question, but assuming you meant "We need to lock THE clock signal", then this could be a challenge do to without affecting SNR. 

    The devices we have that are capable of locking to such a low frequency are not our best performance jitter products.  The locking function could be supported by the AD9549, AD9548, or perhaps the AD9551 or AD9557.  These devices are more typically targeted at non-converter applications in the wired network space, where the 12k to 20M spec you call out is most important.  You could take the output of that device and possibly improve the jitter some by sending it through the AD9523-1 or AD9524, which feature a dual loop configuration where one loop has a narrow LFBW to clean the clock up and the second has a wider LFBW and can upconvert the frequency to your final desired one.

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:35 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin