Hope to provide the firmware source for AD9518-0

Hello.I use AD9518-0 device to
generate
the system clock signal in my project. using the evaluation board circuits, it is more difficult to debug
without firmware code.on the ADI's forum, I find some similarities firmware,
it is very
inconvenient
to modify. whether your company's
ability to
provide the device
firmware source code to help the development of the
project, I want to be able to get help. I wish you prosperity
of the company
.

Parents
  • I used the Evaluation Board AD9518-0 the principle circuit, I want to produce a two-way 600MHz clock signal.

    The circuit board is designed based on evaluation board.

    The absence of the firmware, I the AD9549 firmware.

    Through several tests to find the AD9518 the PID :0XEE11。

    Change the firmware of the AD9549 the PID for 0XEE11 download 68013A, the computer is able to find the driver of the AD9518.But do not know to modify firmware is not applicable AD9518-0, if the AD9518-0 firmware source code, debugging circuit is much more convenient.

Reply
  • I used the Evaluation Board AD9518-0 the principle circuit, I want to produce a two-way 600MHz clock signal.

    The circuit board is designed based on evaluation board.

    The absence of the firmware, I the AD9549 firmware.

    Through several tests to find the AD9518 the PID :0XEE11。

    Change the firmware of the AD9549 the PID for 0XEE11 download 68013A, the computer is able to find the driver of the AD9518.But do not know to modify firmware is not applicable AD9518-0, if the AD9518-0 firmware source code, debugging circuit is much more convenient.

Children
No Data