ADCLK944/948 - low frequency clock input

Hello,

My name is Meir and I am DFAE.

One of my castomers is interested in ADCLK944/948 clock distributor due to his low jitter and low skew performance. The input clock frequency  range: 1Hz - 100MHz with a rise time of 10nsec.

My questions are:

1. Is the ADCLK944/948 may drive the clock of 1Hz-100MHz without any degradation? If not, what is the degradation value?

2. What is the minimum clock frequency that the ADCLK944/948 can drive?   

Thanks in advance.

Best Regards,

Meir

Parents Reply Children
No Data