AD9517-0 Evaluation board to drive a prototype board populated with an AD9517-0

Hi everyone,

I am trying to use a "AD9517/PCBZ (Rev B)" evaluation board to drive an AD9517-0 installed in another board designed by us.

The intention is to use the "AD9516/17/18 Evaluation Software, Version 1.1.0" to control/program the AD9517-0 mounted in our board. To do that, we removed the evaluation board AD9517-0 and wire the signals from connector P1 to our board.


Who can I be sure that the communication with the AD9517-0 is correct?

Is it any thing that prevents this setup to work?

Any advise will be really appreciated.

Best regards

GuiX

Parents
  • 0
    •  Analog Employees 
    on Jan 10, 2015 4:14 AM

    Hi GuiX,


    It is worth mentioning that if you are using a 32-bit Windows machine, you can use the original evaluation board flash and version 1.1.0 of the evaluation software without any issues.


    I do not have access to a Windows XP machine at the moment, but I will take a look when I return to the office next week.


    Regards,
    Kyle

Reply
  • 0
    •  Analog Employees 
    on Jan 10, 2015 4:14 AM

    Hi GuiX,


    It is worth mentioning that if you are using a 32-bit Windows machine, you can use the original evaluation board flash and version 1.1.0 of the evaluation software without any issues.


    I do not have access to a Windows XP machine at the moment, but I will take a look when I return to the office next week.


    Regards,
    Kyle

Children
No Data