Post Go back to editing

AD9517 LVPECL output interface to a fanout buffer

Thread Summary

The user asked if a 100 ohm resistor should be kept at the input of an LVDS receiver when using an AD9517-0 LVPECL output to drive it. The final answer from the support engineer indicates that the 100 ohm resistor is not needed and would halve the signal amplitude. The support engineer also noted that the maximum frequency for LVPECL to LVDS conversion is 1.6 GHz, as this is the highest frequency at which the amplitude is sufficient for most LVPECL receivers to function properly.
AI Generated Content

Hello everyone:

I am using one AD9517-0 LVPECL output to drive a fanout buffer to convert the signal to two LDVS signals.

In the AD9517-0 datasheet I can see this figure to interface LVPECL stages:

On the other hand, in the datasheet of the fanout buffer, I can see this other configuration:

My dessign follows the AD recomendation (first schematic) and incorporates R1 to R4 of the second schematic.

Question: Should I keep the 100 Ohn resistor at the imput of the receiver (as proposed in the AD schematic)?

Thanks in advance

Regards

GuiX

Parents
  • Hi GuiX,

    Our datasheet figure with the 100 ohm differential termination assumes that the LVPECL receiver is self biased.  The clock buffer figure (2D) is biasing the receiver to a ~2V common mode using an external 3.3V supply and resistor divider and is also setting the input impedance to ~50 ohms (84||125) to match each trace to the receiver.

    The 100ohm differential resistor is not needed when using the clock buffer termination diagram.  Please let me know if I can help further.

    Regards,
    Kyle

Reply
  • Hi GuiX,

    Our datasheet figure with the 100 ohm differential termination assumes that the LVPECL receiver is self biased.  The clock buffer figure (2D) is biasing the receiver to a ~2V common mode using an external 3.3V supply and resistor divider and is also setting the input impedance to ~50 ohms (84||125) to match each trace to the receiver.

    The 100ohm differential resistor is not needed when using the clock buffer termination diagram.  Please let me know if I can help further.

    Regards,
    Kyle

Children
No Data