Post Go back to editing

Alternate crystal frequency for AD9575

I need to synthesize a 135 MHz very low-phase noise differential (LVDS or LVPECL) clock for my present application.

The AD9575 looks like a convenient choice, though the datasheet indicates that it wants one of three specific reference clocks/crystals as input. From my calculations, in its 6.25 or 6.375 multiplier ratios, it will generate 135 MHz given a 21.6 MHz or 21.17 MHz clock input.

Question: will this work?

Second question: this device is specified for a maximum reference input of 25.78 MHz -- would it tolerate 27 MHz? Used the times 5 mode, this would also meet my requirements.

Advice is appreciated.

[Data Sheet attached for your convenience]

AD9575.pdf
Parents Reply Children
No Data