AD9522-1
Recommended for New Designs
The AD9522-11 provides a multioutput clock distribution function with subpicosecond jitter performance, along with an on-chip PLL and VCO. The on-chip...
Datasheet
AD9522-1 on Analog.com
Hi,
Looking for a support on AD9522-1 input reference clock. We are using singled ended reference clock[one from FPGA, one from oscillator], with AC coupling and AD9522 internal DC offset is off.
When we probed on the REF_IN pin, there is a -0.4V offset in the clock signal. Can you please check it?
Attaching the schematic and waveform of the corresponding section.
Thank you,
Regards,
Sneha
Hello Sneha,
This behavior is expected. When in AC-coupled, single-ended mode, the user must either use the internal DC-bias mode or provide DC-biasing so that the input clock goes from 0 to 3.3V.
The reason we added the DC-bias mode to the SE input is to avoid this issue.
-Paul Kern