Please Help:  how to get the clk out from the AD9554

I just only use Ref A(19.2MHz), left the RefB/RefC/RefD open (I just put the 0.01MHz for refb due to the GUI ask for 1 input for the other 3Ref input),  4chanel total 8port output 167.33166MHz, the following fig shows, system clock is 49.152Mhz

Does these setting work for board?

this is 49.152MHz system clk (I just get the single-end data,which is differetial input)

here is the 19.2MHz clk for the Ref A input

   we am just debug the board use the AD9554 for the OTU2 ref clock,   the processor could access AD9554 by I2C port. and could get the Device ID, also could read and write Reg 0x200 and 0x201 ..

we don't  use the EPROM, so left the M-pin open.

we just set the register from register0x200~register0x365.

But there are no output clk at the portA/B/C, Is there any other setting we need to config to get the output clock from AD9554?

  

  

     we use the wizard to get the NonDefault register map(111 nondefault reg), last pic shows.  we only could set part of these reg, such as Reg0x200,Reg0x204,~reg0x346,  while we can not set the other regs,  from 0x400 to the end,

any clue why we can not change the nondefault register setting?

Is there any setting we should pay more attention?

Thank you in advance

  

 

  •   
  •      
Parents
  • Neil

       Thank you for response and explanation.

        I tried the operation based on your recommendation, it do works for 2 output channel(chanel 0 and channel 2 could locked), while the other 2 channel not locked(system clk locked, DLL locked , APLL not locked).

        Any clue about the 2 channel out of lock?

        all the register setting is as following shows(Sorry I don't find how to upload file, just copy all the setting I use):

    we only have one ref clock(19.2MHz) to the REFA, the other 3 ref clk input(REFB/REFC/REFD) are open(not connect), system input clk is 49.152MHz. the 19.2MHz input and 49.152MHz wavform please refer to the yesterday's post.

    <detailed setup information>
    -- System Clock --
        Input Freq: 49.152 MHz
        Input Type: Crystal Resonator
        J: x2
        Pfd Freq: 98.304 MHz
        K: 24
        VCO Freq: 2.359296 GHz
    ------------------
    -- Reference Inputs --
    - Ref A -    Input Freq: 19.2 MHz
        Ra: 96
        Dpfd Freq: 200.0 kHz
    - Ref B -    Input Freq: 19.44 MHz
        Rb: 1
        Dpfd Freq: 19.44 MHz
    - Ref C -    Input Freq: 19.44 MHz
        Rc: 1
        Dpfd Freq: 19.44 MHz
    - Ref D -    Input Freq: 19.44 MHz
        Rd: 1
        Dpfd Freq: 19.44 MHz
    ----------------------
    -- Channel 0 --
    - Dpll -
       Ref A
        N 0a: 1,568
        Frac 0a: 58
        Mod 0a: 79
        LBW 0a: 50.0
       Ref B
        N 0b: 1
        Frac 0b:
        Mod 0b:
        LBW 0b: 50.0
       Ref C
        N 0c: 1
        Frac 0c:
        Mod 0c:
        LBW 0c: 50.0
       Ref D
        N 0d: 1
        Frac 0d:
        Mod 0d:
        LBW 0d: 50.0
       DCO
        Int 0: 7
        FTW 0: 558,071,270
    - Apll -
        Apfd 0 Freq: 313.746835 MHz
        M 0: 8
        VCO 0 Freq: 2,509.974683 MHz
        P 0: 3
        Qa 0: 5
        Out 0A Freq: 167.331646 MHz
        Qb 0: 5
        Out 0B Freq: 167.331646 MHz
    ---------------
    -- Channel 1 --
    - Dpll -
       Ref A
        N 1a: 1,521
        Frac 1a: 171
        Mod 1a: 869
        LBW 1a: 50.0
       Ref B
        N 1b: 1
        Frac 1b:
        Mod 1b:
        LBW 1b: 50.0
       Ref C
        N 1c: 1
        Frac 1c:
        Mod 1c:
        LBW 1c: 50.0
       Ref D
        N 1d: 1
        Frac 1d:
        Mod 1d:
        LBW 1d: 50.0
       DCO
        Int 1: 7
        FTW 1: 810,392,021
    - Apll -
        Apfd 1 Freq: 304.239356 MHz
        M 1: 11
        VCO 1 Freq: 3,346.632911 MHz
        P 1: 4
        Qa 1: 5
        Out 1A Freq: 167.331646 MHz
        Qb 1: 5
        Out 1B Freq: 167.331646 MHz
    ---------------
    -- Channel 2 --
    - Dpll -
       Ref A
        N 2a: 1,568
        Frac 2a: 58
        Mod 2a: 79
        LBW 2a: 50.0
       Ref B
        N 2b: 1
        Frac 2b:
        Mod 2b:
        LBW 2b: 50.0
       Ref C
        N 2c: 1
        Frac 2c:
        Mod 2c:
        LBW 2c: 50.0
       Ref D
        N 2d: 1
        Frac 2d:
        Mod 2d:
        LBW 2d: 50.0
       DCO
        Int 2: 7
        FTW 2: 558,071,270
    - Apll -
        Apfd 2 Freq: 313.746835 MHz
        M 2: 16
        VCO 2 Freq: 5,019.949367 MHz
        P 2: 5
        Qa 2: 6
        Out 2A Freq: 167.331646 MHz
        Qb 2: 6
        Out 2B Freq: 167.331646 MHz
    ---------------
    -- Channel 3 --
    - Dpll -
       Ref A
        N 3a: 1,608
        Frac 3a: 984
        Mod 3a: 1,027
        LBW 3a: 50.0
       Ref B
        N 3b: 1
        Frac 3b:
        Mod 3b:
        LBW 3b: 50.0
       Ref C
        N 3c: 1
        Frac 3c:
        Mod 3c:
        LBW 3c: 50.0
       Ref D
        N 3d: 1
        Frac 3d:
        Mod 3d:
        LBW 3d: 50.0
       DCO
        Int 3: 7
        FTW 3: 356,214,669
    - Apll -
        Apfd 3 Freq: 321.791626 MHz
        M 3: 13
        VCO 3 Freq: 4,183.291139 MHz
        P 3: 5
        Qa 3: 5
        Out 3A Freq: 167.331646 MHz
        Qb 3: 5
        Out 3B Freq: 167.331646 MHz
    ---------------
    </detailed setup information>

    <registers>
    Register (Hex), Value (Hex), Value (Dec)
    0x200,  0x18,  24
    0x201,  0x09,  9
    0x204,  0xEE,  238
    0x205,  0x02,  2
    0x301,  0x5F,  95
    0x304,  0x85,  133
    0x305,  0xBA,  186
    0x306,  0x1A,  26
    0x307,  0x03,  3
    0x400,  0xE6,  230
    0x401,  0x7D,  125
    0x402,  0x43,  67
    0x403,  0x21,  33
    0x431,  0x08,  8
    0x434,  0x03,  3
    0x438,  0x04,  4
    0x43c,  0x04,  4
    0x440,  0x01,  1
    0x441,  0xF4,  244
    0x442,  0x01,  1
    0x444,  0x1F,  31
    0x445,  0x06,  6
    0x447,  0x3A,  58
    0x44a,  0x4F,  79
    0x44e,  0xF4,  244
    0x44f,  0x01,  1
    0x45b,  0xF4,  244
    0x45c,  0x01,  1
    0x468,  0xF4,  244
    0x469,  0x01,  1
    0x500,  0xD5,  213
    0x501,  0x99,  153
    0x502,  0x4D,  77
    0x503,  0x30,  48
    0x531,  0x0B,  11
    0x534,  0x04,  4
    0x538,  0x04,  4
    0x53c,  0x04,  4
    0x540,  0x01,  1
    0x541,  0xF4,  244
    0x542,  0x01,  1
    0x544,  0xF0,  240
    0x545,  0x05,  5
    0x547,  0xAB,  171
    0x54a,  0x65,  101
    0x54b,  0x03,  3
    0x54e,  0xF4,  244
    0x54f,  0x01,  1
    0x55b,  0xF4,  244
    0x55c,  0x01,  1
    0x568,  0xF4,  244
    0x569,  0x01,  1
    0x600,  0xE6,  230
    0x601,  0x7D,  125
    0x602,  0x43,  67
    0x603,  0x21,  33
    0x631,  0x10,  16
    0x634,  0x05,  5
    0x638,  0x05,  5
    0x63c,  0x05,  5
    0x640,  0x01,  1
    0x641,  0xF4,  244
    0x642,  0x01,  1
    0x644,  0x1F,  31
    0x645,  0x06,  6
    0x647,  0x3A,  58
    0x64a,  0x4F,  79
    0x64e,  0xF4,  244
    0x64f,  0x01,  1
    0x65b,  0xF4,  244
    0x65c,  0x01,  1
    0x668,  0xF4,  244
    0x669,  0x01,  1
    0x700,  0x8D,  141
    0x701,  0x67,  103
    0x702,  0x3B,  59
    0x703,  0x15,  21
    0x731,  0x0D,  13
    0x734,  0x05,  5
    0x738,  0x04,  4
    0x73c,  0x04,  4
    0x740,  0x01,  1
    0x741,  0xF4,  244
    0x742,  0x01,  1
    0x744,  0x47,  71
    0x745,  0x06,  6
    0x747,  0xD8,  216
    0x748,  0x03,  3
    0x74a,  0x03,  3
    0x74b,  0x04,  4
    0x74e,  0xF4,  244
    0x74f,  0x01,  1
    0x75b,  0xF4,  244
    0x75c,  0x01,  1
    0x768,  0xF4,  244
    0x769,  0x01,  1
    0xFFF,  0xF9,  249
    0x1488,  0x03,  3
    0x1588,  0x03,  3
    0x1688,  0x03,  3
    0x1788,  0x03,  3
    0xF,  0x01,  1
    0xFFF,  0x00,  0
    </registers>

    <frequencies>
    19200000;19440000;19440000;19440000;49152000
    </frequencies>

    <ftwfreq>
    155520000;19440000;19440000;19440000;155520000;155520000;155520000;155520000;49.152
    </ftwfreq>

    <ftwfecref>
    10;81;1;1;1;1;1;1
    </ftwfecref>

    <ftwfecout>
    85;79;1;1;85;79;1;1;85;79;1;1;85;79;1;1
    </ftwfecout>

    <ftwenref>
    True;True;True;True;False;False;False;False;False;False;False;False;False;False;False;False;True
    </ftwenref>

    <ftwlbwref>
    50;50;50;50
    </ftwlbwref>

    <ftwselref>
    0;1;1;1
    </ftwselref>

Reply
  • Neil

       Thank you for response and explanation.

        I tried the operation based on your recommendation, it do works for 2 output channel(chanel 0 and channel 2 could locked), while the other 2 channel not locked(system clk locked, DLL locked , APLL not locked).

        Any clue about the 2 channel out of lock?

        all the register setting is as following shows(Sorry I don't find how to upload file, just copy all the setting I use):

    we only have one ref clock(19.2MHz) to the REFA, the other 3 ref clk input(REFB/REFC/REFD) are open(not connect), system input clk is 49.152MHz. the 19.2MHz input and 49.152MHz wavform please refer to the yesterday's post.

    <detailed setup information>
    -- System Clock --
        Input Freq: 49.152 MHz
        Input Type: Crystal Resonator
        J: x2
        Pfd Freq: 98.304 MHz
        K: 24
        VCO Freq: 2.359296 GHz
    ------------------
    -- Reference Inputs --
    - Ref A -    Input Freq: 19.2 MHz
        Ra: 96
        Dpfd Freq: 200.0 kHz
    - Ref B -    Input Freq: 19.44 MHz
        Rb: 1
        Dpfd Freq: 19.44 MHz
    - Ref C -    Input Freq: 19.44 MHz
        Rc: 1
        Dpfd Freq: 19.44 MHz
    - Ref D -    Input Freq: 19.44 MHz
        Rd: 1
        Dpfd Freq: 19.44 MHz
    ----------------------
    -- Channel 0 --
    - Dpll -
       Ref A
        N 0a: 1,568
        Frac 0a: 58
        Mod 0a: 79
        LBW 0a: 50.0
       Ref B
        N 0b: 1
        Frac 0b:
        Mod 0b:
        LBW 0b: 50.0
       Ref C
        N 0c: 1
        Frac 0c:
        Mod 0c:
        LBW 0c: 50.0
       Ref D
        N 0d: 1
        Frac 0d:
        Mod 0d:
        LBW 0d: 50.0
       DCO
        Int 0: 7
        FTW 0: 558,071,270
    - Apll -
        Apfd 0 Freq: 313.746835 MHz
        M 0: 8
        VCO 0 Freq: 2,509.974683 MHz
        P 0: 3
        Qa 0: 5
        Out 0A Freq: 167.331646 MHz
        Qb 0: 5
        Out 0B Freq: 167.331646 MHz
    ---------------
    -- Channel 1 --
    - Dpll -
       Ref A
        N 1a: 1,521
        Frac 1a: 171
        Mod 1a: 869
        LBW 1a: 50.0
       Ref B
        N 1b: 1
        Frac 1b:
        Mod 1b:
        LBW 1b: 50.0
       Ref C
        N 1c: 1
        Frac 1c:
        Mod 1c:
        LBW 1c: 50.0
       Ref D
        N 1d: 1
        Frac 1d:
        Mod 1d:
        LBW 1d: 50.0
       DCO
        Int 1: 7
        FTW 1: 810,392,021
    - Apll -
        Apfd 1 Freq: 304.239356 MHz
        M 1: 11
        VCO 1 Freq: 3,346.632911 MHz
        P 1: 4
        Qa 1: 5
        Out 1A Freq: 167.331646 MHz
        Qb 1: 5
        Out 1B Freq: 167.331646 MHz
    ---------------
    -- Channel 2 --
    - Dpll -
       Ref A
        N 2a: 1,568
        Frac 2a: 58
        Mod 2a: 79
        LBW 2a: 50.0
       Ref B
        N 2b: 1
        Frac 2b:
        Mod 2b:
        LBW 2b: 50.0
       Ref C
        N 2c: 1
        Frac 2c:
        Mod 2c:
        LBW 2c: 50.0
       Ref D
        N 2d: 1
        Frac 2d:
        Mod 2d:
        LBW 2d: 50.0
       DCO
        Int 2: 7
        FTW 2: 558,071,270
    - Apll -
        Apfd 2 Freq: 313.746835 MHz
        M 2: 16
        VCO 2 Freq: 5,019.949367 MHz
        P 2: 5
        Qa 2: 6
        Out 2A Freq: 167.331646 MHz
        Qb 2: 6
        Out 2B Freq: 167.331646 MHz
    ---------------
    -- Channel 3 --
    - Dpll -
       Ref A
        N 3a: 1,608
        Frac 3a: 984
        Mod 3a: 1,027
        LBW 3a: 50.0
       Ref B
        N 3b: 1
        Frac 3b:
        Mod 3b:
        LBW 3b: 50.0
       Ref C
        N 3c: 1
        Frac 3c:
        Mod 3c:
        LBW 3c: 50.0
       Ref D
        N 3d: 1
        Frac 3d:
        Mod 3d:
        LBW 3d: 50.0
       DCO
        Int 3: 7
        FTW 3: 356,214,669
    - Apll -
        Apfd 3 Freq: 321.791626 MHz
        M 3: 13
        VCO 3 Freq: 4,183.291139 MHz
        P 3: 5
        Qa 3: 5
        Out 3A Freq: 167.331646 MHz
        Qb 3: 5
        Out 3B Freq: 167.331646 MHz
    ---------------
    </detailed setup information>

    <registers>
    Register (Hex), Value (Hex), Value (Dec)
    0x200,  0x18,  24
    0x201,  0x09,  9
    0x204,  0xEE,  238
    0x205,  0x02,  2
    0x301,  0x5F,  95
    0x304,  0x85,  133
    0x305,  0xBA,  186
    0x306,  0x1A,  26
    0x307,  0x03,  3
    0x400,  0xE6,  230
    0x401,  0x7D,  125
    0x402,  0x43,  67
    0x403,  0x21,  33
    0x431,  0x08,  8
    0x434,  0x03,  3
    0x438,  0x04,  4
    0x43c,  0x04,  4
    0x440,  0x01,  1
    0x441,  0xF4,  244
    0x442,  0x01,  1
    0x444,  0x1F,  31
    0x445,  0x06,  6
    0x447,  0x3A,  58
    0x44a,  0x4F,  79
    0x44e,  0xF4,  244
    0x44f,  0x01,  1
    0x45b,  0xF4,  244
    0x45c,  0x01,  1
    0x468,  0xF4,  244
    0x469,  0x01,  1
    0x500,  0xD5,  213
    0x501,  0x99,  153
    0x502,  0x4D,  77
    0x503,  0x30,  48
    0x531,  0x0B,  11
    0x534,  0x04,  4
    0x538,  0x04,  4
    0x53c,  0x04,  4
    0x540,  0x01,  1
    0x541,  0xF4,  244
    0x542,  0x01,  1
    0x544,  0xF0,  240
    0x545,  0x05,  5
    0x547,  0xAB,  171
    0x54a,  0x65,  101
    0x54b,  0x03,  3
    0x54e,  0xF4,  244
    0x54f,  0x01,  1
    0x55b,  0xF4,  244
    0x55c,  0x01,  1
    0x568,  0xF4,  244
    0x569,  0x01,  1
    0x600,  0xE6,  230
    0x601,  0x7D,  125
    0x602,  0x43,  67
    0x603,  0x21,  33
    0x631,  0x10,  16
    0x634,  0x05,  5
    0x638,  0x05,  5
    0x63c,  0x05,  5
    0x640,  0x01,  1
    0x641,  0xF4,  244
    0x642,  0x01,  1
    0x644,  0x1F,  31
    0x645,  0x06,  6
    0x647,  0x3A,  58
    0x64a,  0x4F,  79
    0x64e,  0xF4,  244
    0x64f,  0x01,  1
    0x65b,  0xF4,  244
    0x65c,  0x01,  1
    0x668,  0xF4,  244
    0x669,  0x01,  1
    0x700,  0x8D,  141
    0x701,  0x67,  103
    0x702,  0x3B,  59
    0x703,  0x15,  21
    0x731,  0x0D,  13
    0x734,  0x05,  5
    0x738,  0x04,  4
    0x73c,  0x04,  4
    0x740,  0x01,  1
    0x741,  0xF4,  244
    0x742,  0x01,  1
    0x744,  0x47,  71
    0x745,  0x06,  6
    0x747,  0xD8,  216
    0x748,  0x03,  3
    0x74a,  0x03,  3
    0x74b,  0x04,  4
    0x74e,  0xF4,  244
    0x74f,  0x01,  1
    0x75b,  0xF4,  244
    0x75c,  0x01,  1
    0x768,  0xF4,  244
    0x769,  0x01,  1
    0xFFF,  0xF9,  249
    0x1488,  0x03,  3
    0x1588,  0x03,  3
    0x1688,  0x03,  3
    0x1788,  0x03,  3
    0xF,  0x01,  1
    0xFFF,  0x00,  0
    </registers>

    <frequencies>
    19200000;19440000;19440000;19440000;49152000
    </frequencies>

    <ftwfreq>
    155520000;19440000;19440000;19440000;155520000;155520000;155520000;155520000;49.152
    </ftwfreq>

    <ftwfecref>
    10;81;1;1;1;1;1;1
    </ftwfecref>

    <ftwfecout>
    85;79;1;1;85;79;1;1;85;79;1;1;85;79;1;1
    </ftwfecout>

    <ftwenref>
    True;True;True;True;False;False;False;False;False;False;False;False;False;False;False;False;True
    </ftwenref>

    <ftwlbwref>
    50;50;50;50
    </ftwlbwref>

    <ftwselref>
    0;1;1;1
    </ftwselref>

Children
No Data