Post Go back to editing

AD9517-3 SPI Interface

Thread Summary

The user encountered issues with the AD9517-3 not responding in a 4-wire interface and the PLL not locking. The problem was resolved by writing 0x19 to address 0x000, setting the 4-wire interface, and adjusting the loop filter components to match the eval board configuration.
AI Generated Content

Hello,

     For a new project we are using the AD9517-3. Prior to this we have successfully programmed and used the AD9523-1.

The problem right now is that there is no response from the AD9517-3 in a 4 wire interface.

The steps we follow are as follows:

1) Write 0x19 to address 0x000 (long instruction mode, 4 wire interface).

2) Write 0x01 to address 0x232 (transfer to active register set).

3) Read from 0x003 (device ID).

We are unable to get anything out of the SDO pin.

The schematic and pcb connections have been verified. We are using exactly the same interface that worked for AD9523-1 to talk to the AD9517-3.

Thank you for your help in advance,

  • Hello,

         The problem of not getting a response has been fixed. d153 had to be written at h0.

    The problem now is that the PLL is not locked or the output freq is not correct.

    We have a 200MHz differential reference in and the loop filter is same as that on the eval board.

    Reset is pulled high and Ref_Sel is tied low.

    After writing all the registers once 0x018(0) is set to 1.

    Then 0x01F is read and the result is 0x0E (VCO cal not done and no lock).

    CP out pin is at 0V and bypass pin cap is at ~2.6V.

    Thank you for your help,

    The register settings are as follows: (For 125MHz CMOS out on o/p5)

    AD9516/17/18 Register Map File, Rev 1.0

    Addr(Hex)     Value(Bin)    Value(Hex)

    0000          00011000      18

    0001          00000000      00

    0002          00010000      10

    0003          01010011      53

    0004          00000000      00

    0010          01111100      7C

    0011          11001000      C8

    0012          00000000      00

    0013          00000000      00

    0014          01111101      7D

    0015          00000000      00

    0016          00000101      05

    0017          00000000      00

    0018          00000110      06

    0019          00000000      00

    001A          00000000      00

    001B          00000000      00

    001C          01000000      87

    001D          00000000      00

    001E          00000000      00

    001F          00001110      0E

    00A0          00000001      01

    00A1          00000000      00

    00A2          00000000      00

    00A3          00000001      01

    00A4          00000000      00

    00A5          00000000      00

    00A6          00000001      01

    00A7          00000000      00

    00A8          00000000      00

    00A9          00000001      01

    00AA          00000000      00

    00AB          00000000      00

    00F0          00001010      0A

    00F1          00001010      0A

    00F2          00001000      08

    00F3          00001010      0A

    00F4          00001010      0A

    00F5          00001010      0A

    0140          01000011      43

    0141          01011010      5A

    0142          01000011      43

    0143          01000011      43

    0190          00000000      00

    0191          10000000      80

    0192          00000000      00

    0193          10111011      BB

    0194          00000000      00

    0195          00000000      00

    0196          00000000      00

    0197          00000000      00

    0198          00000000      00

    0199          00000000      00

    019A          00000000      00

    019B          00000000      00

    019C          00000000      00

    019D          00000000      00

    019E          00100010      22

    019F          00000000      00

    01A0          00010001      11

    01A1          00000000      00

    01A2          00000000      00

    01A3          00000000      00

    01E0          00000010      02

    01E1          00000010      02

    0230          00000000      00

    0231          00000000      00

    0232          00000000      00

  • Hi Shashank,

    I believe this issue was resolved by working with you one-on-one, and changing the loop filter components.

    Please let me know if I'm mistaken.

    -Paul Kern

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin