AD 9520 EEprom

Dear all,

I'm having problems in programming the EEPROM of the AD9520.

I use the SPI to program the PLL.

When I try to configure directly the PLL via SPI, it works and the wanted clock is at the output;

I can see the lock signal at '1' and everything goes fine.

When I try to program the EEPROM, problems start.

I am doing as follows:

1) I program the PLL as I want ( and I see the lock at '1'); in particular, I set the status pin in such a way to see the EEPROM status

2) I set 0xb02[0] at '1'

3) I set 0xb03[0] at '1'

4) I set an update with 0x232[0] at '1'

I do not see the status pin at '1' (as it should be during the EEPROM programming) and it looks like the eeprom is not programmed at all; if I try to give a self-clearing soft reset (0x000[5]), with the EEPROM pin high I do not see the new configuration loaded.

The strange part is that if I try to set 0xb02[0] at '1', set 0xb02[0] at '1' and then 0x232[0] at '1', as soon as I try to read again 0xb02[0] it is at '0' ( it looks like the EEPROM write is not enabled). I also tried to set 0xb02[0] at '1' and update but when I read it back, it is at '0'.

Any ideas?

Regards.

Alberto

Parents
No Data
Reply
  • Hello Alberto,

    I'll need to look at this more closely, but it appears that your procedure is correct, although I would omit the R0x0232=0x01 (the third step) when burning the EEPROM, as I'm pretty sure that the EEPROM burn bit are live.

    At that point, you should be able to monitor the EEPROM status bit.

    I'll look at this more closely once I'm back in the office.

    -Paul Kern

Children
No Data