Hello,
we design a system with ad9518-1, but AD9518-1 pin outputs DC 1.6V, and the complement pin output DC 2.4V, no clock output, why?
Thank you!
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
AD9518-1
Recommended for New Designs
The AD9518-11 The AD9518-11 provides a multi-output clock distribution function with subpicosecond jitter performance, along with an on chip PLL and VCO...
Datasheet
AD9518-1 on Analog.com
Hello,
we design a system with ad9518-1, but AD9518-1 pin outputs DC 1.6V, and the complement pin output DC 2.4V, no clock output, why?
Thank you!
Hello Kerb,
If the output is static, check the following:
1. Is the SYNCb pin low?
2. Are you using the PLL? If so, is it locked?
Here's a link to the eval software user guide, and it discusses how to bring up the part in general:
http://www.analog.com/media/en/technical-documentation/user-guides/UG-075.pdf
My guess is that either the PLL isn't configured correctly and isn't locked, or that the SYNCb pin is low.
-Paul Kern