The HMC6832 data sheet states that its differential output voltage swing is 721mVpp typ when used in 3V3 LVPECL mode. To check: presumably, this is the swing of each output in the differential pair, so that the full differential output swing is 1.4Vpp into 100Ohms, right? Is that correct? In other words, is the output voltage swing of the HMC6832 similar to other ICs like the ADCLK948?