Hello,
I'm working with the EVAL-AD9554 board as jitter cleanup for my high-precision ADC (AD7760 with 24 bits). I was wondering if there is a way to get CMOS logic from clock outputs? Actually, I need 0 to 3.3 V clock to feed the AD7760. As I searched on the main web page for EVAL-AD9554 there was no documentation or application note about its configurations and that's why I'm confused. It would be highly appreciated if anybody can help me in this matter. Thanks