I have updated the eval board software using AD9516_17_18_Evaluation_USB_Flash_Programmer.
I can communicate with the board using the AD9516_17_18_evaluation_software_full_install
I have manually installed the drivers on the computer so the board is identified as "ADI Evaluation System (LRFDev)"
BUT the "Program Chip" is grayed out.
I see that I should check that the ADIsimCLK actually supports the board in question but I have no idea of where to find such information.