HMC7044

Hi,

I have some questions about the component:

1. what should be the input configuration to get into osc-in in LVDS format?

2. In the D\S is mentioned:

For a 2.1 V commonmode, 50 Ω single-ended source, the input limit of 2.8 V allows ~700 mV of amplitude, or 6 dBm of maximum reference power.

My question is about the differential input. Does The limit of 1.4Vp-p is differential or refer to each leg (which bring us to 2.8Vp-p differential)?

3. What should I connect to the unused leg for single-ended input (A or B configuration)?  

Thanks,

Asaf



.
[edited by: AS709 at 2:59 PM (GMT 0) on 27 Jun 2020]
Parents Reply Children