Hi,
I have some questions about the component:
1. what should be the input configuration to get into osc-in in LVDS format?
2. In the D\S is mentioned:
For a 2.1 V commonmode, 50 Ω single-ended source, the input limit of 2.8 V allows ~700 mV of amplitude, or 6 dBm of maximum reference power.
My question is about the differential input. Does The limit of 1.4Vp-p is differential or refer to each leg (which bring us to 2.8Vp-p differential)?
3. What should I connect to the unused leg for single-ended input (A or B configuration)?
Thanks,
Asaf
Hi Asaf,
1) For AC coupled LVDS input, you need to enable AC coupled input, disable 100 ohm internal termination and enable Hi-Z input. Also, you need to put 100 ohm termination resistance between positive…
what is the signal to signal jitter of the same output (using an external VCO input)?
??