Post Go back to editing

LTC6953 vs LTC6952 multi-stage sync

Thread Summary

The user is implementing a refclk/sysref distribution scheme with the LTC6953 and LTC6952 in a 3-stage configuration. The final answer confirms that the SYSREF signal at the end of the chain (stage 3) is guaranteed to assert on the same clock edge across the array of stage 2 devices, using the pass-thru mode. The solution involves programming the devices with specific SPI settings and ensuring proper synchronization through the SSRQ bit. The accompanying answers clarify that the setup/hold requirements for the SRQ signal relative to IN must be met, and the 1ms requirement for asserting SSRQ is to ensure synchronization in pass-thru mode.
AI Generated Content

Hello - I am trying to implement the refclk/sysref distribution scheme shown in the LTC6953 datasheet on pg. 54.  The LTC6952 datasheet specifies the relationship between the IN± and EZS_SRQ± lines in PARSYNC mode.  The LTC6953 doesn't support PARSYNC mode and only lists a typical minimum time of 1ms to assert EZS_SRQ±.

Is the SYSREF signal at the end of the chain (stage 3 on page 54) guaranteed to assert on the same clock edge across the entire array of stage 2 devices? 

Thanks,

Nick

  • Hi Nick,

    Correct, by definition PARSYNC is away to synchronize a device with a PLL.  In the page 54 example all the stage 2 sysref's will be aligned to each other as long as their DDELs are set to the same value.

    I attached a video of this setup in action.  It uses the DC2430 w/ Linduino

    https://drive.google.com/file/d/10AWCXTT0mKU1-ZdMZKFiLw_np-YKRWmL/view?usp=sharing

  • Hi Chris,

    thanks for the response.  I’m still trying wrap my head around the clock/sysref distribution.

    the 6952 data sheet specifies a setup/hold requirement for srq relative to in.  The 6953 says to assert ssrq for 1ms.  Can 6953 really guarantee sync without a setup and hold?

    The 1ms req seems to imply that the middle stage must be configured for pass thru mode (or else how do you get a big enough divider to meet the 1ms req at the final stage?

    thanks,

    nick

  • Hey Nick,

    I apologize, I looked at page 53.  Page 54 is the 3 stage Sync example.  Jon is going to setup a call.  I need to look on my computer for the code I used to perform this.  I think that will be the most straight forward thing to follow.  I'll need a day to locate the code... Slight smile

  • Nick,

    I think the short answer is it uses the passthru mode.

    In the LTC6952Wizard, you can select 'File --> Load Settings'.  In the 'LTC6952 Typical Applications' there are 3 files, that provide the initial state for the 3 stage parallelsync example.

    From there you should be able to follow the steps in the datasheet (page 55 ltc6953, or page 77 ltc6952 datasheet), for programming instructions.

    Below is a snippet of Arduino code that I used for this example.  I've also attached the original Arduino code, but you'll need to download the LTSketchbook from analog.com to use this (For the support files).  You can put these directory structure in the LTSketchbook WIP folder.   (Note this uses the DC2430 board connected to 3 LTC6953s and 2 LTC6952s) https://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/DC2430AF.PDF

    LTC6952_590.zip.

    /* ---------------------------------------------------------------------
    ParallelSync_3Stage_SyncPassthru() - Function performs the 3 Stage
    ParallelSync with Pass thru. See datasheet for block diagram.
    --------------------------------------------------------------------- */
    void ParallelSync_3Stage_SyncPassthru() {
    uint8_t LTC695x_lkup_tbl[5][LTC695x_NUM_REGADDR] = { //!< the following settings assume a 100MHz reference input
    #if 1
    /* these register settings are for a typical use case */
    /* LTC6953 stage 1, DC2430 site 0 */ {0x25, 0x88, 0x02, 0xff, 0xf0, 0x30, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x13},
    /* LTC6953 #1 stage 2, DC2430 site 3 */ {0x25, 0x88, 0x00, 0xff, 0xf0, 0x3c, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x38, 0x80, 0x00, 0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x13},
    /* LTC6953 #2 stage 2, DC2430 site 4 */ {0x25, 0x88, 0x00, 0xff, 0xf0, 0x3c, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x38, 0x80, 0x00, 0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x13},
    /* LTC6952 #1 stage 3, DC2430 site 6 */ {0x15, 0xaa, 0x08, 0x22, 0x82, 0x08, 0xcc, 0x01, 0x00, 0x28, 0x13, 0x06, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x00, 0x00, 0xf8, 0x80, 0x20, 0x00, 0x99, 0x80, 0x00, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x12},
    /* LTC6952 #2 stage 3, DC2430 site 7 */ {0x15, 0xaa, 0x08, 0x22, 0x82, 0x08, 0xcc, 0x01, 0x00, 0x28, 0x13, 0x06, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x00, 0x00, 0xf8, 0x80, 0x20, 0x00, 0x99, 0x80, 0x00, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x12}
    }; //!< LTC6952 Configuration look-up table
    #else
    /* these register settings had dividers at every stage of the reference path - used to prove out worst case sync methods */
    /* LTC6953 stage 1, DC2430 site 0 */ {0x25, 0x88, 0x00, 0xff, 0xf0, 0x30, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x08, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x02, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x08, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x02, 0x00, 0x00, 0x00, 0x00, 0x00, 0x13},
    /* LTC6953 #1 stage 2, DC2430 site 3 */ {0x25, 0x88, 0x00, 0xff, 0xf0, 0x3c, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x08, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x02, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x38, 0x80, 0x00, 0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x13},
    /* LTC6953 #2 stage 2, DC2430 site 4 */ {0x25, 0x88, 0x00, 0xff, 0xf0, 0x3c, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x08, 0x80, 0x00, 0x00, 0x08, 0xc0, 0x02, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x38, 0x80, 0x00, 0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x13},
    /* LTC6952 #1 stage 3, DC2430 site 6 */ {0x15, 0xaa, 0x08, 0x22, 0x82, 0x08, 0xcc, 0x02, 0x01, 0x40, 0x13, 0x06, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x00, 0x00, 0xf8, 0x80, 0x20, 0x00, 0x99, 0x80, 0x00, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x12},
    /* LTC6952 #2 stage 3, DC2430 site 7 */ {0x15, 0xaa, 0x08, 0x22, 0x82, 0x08, 0xcc, 0x02, 0x01, 0x40, 0x13, 0x06, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x18, 0x00, 0x38, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x00, 0x00, 0xf8, 0x80, 0x20, 0x00, 0x99, 0x80, 0x00, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x9c, 0xe0, 0x1f, 0x00, 0x00, 0x80, 0x20, 0x00, 0x12}
    }; //!< LTC6952 Configuration look-up table
    #endif
    uint8_t LTC695x_Site_list[5] = {0,3,4,6,7}; /* site mirrors look up LTC695x_lkup_tbl location */
    uint16_t DC2430_Site_list[8] ={6953,-1,-1,6953,6953,-1,6952,6952};
    uint8_t DC2430_ParallelSync_StageNum[8] = {1,-1,-1,2,2,-1,3,3};
    uint8_t DC2430_ParallelSync_DevNum[8] = {1,-1,-1,1,2,-1,1,2};
    uint8_t *rx; /* for SPI writes */
    uint8_t val_temp; /* for SPI writes */
    int array_loc;
    uint8_t field_num;
    long field_val;
    uint16_t user_command; // User input command

    /* STEP 1: VERIFY DEMO BOARD CONNECTIONS ARE CORRECT */
    DC2430_Bin = 1; // initialize DC2430_Bin
    /* confirms DC2430 & DC2026 uses the correct settings */
    DC2430_test_supply(); // if DC2430 connect and setup properly, then returns global DC2430_Bin=1
    DC2430_SiteCheck(DC2430_Site_list,DC2430_ParallelSync_StageNum,DC2430_ParallelSync_DevNum);
    // if DC2430 connect and setup properly, then returns global DC2430_Bin=1
    Serial.flush();

    if (DC2430_Bin==1) {
    /* STEP DEBUG: Set all devices to Power up state */
    for (array_loc=0; array_loc<5; array_loc++) {
    changeDC2430site(LTC695x_Site_list[array_loc]); // switch DC2430 site
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_POR, 1); /* resets all devices every run */
    } /* end of for loop - array_loc... */

    /* STEP 2: Program Initial SPI settings for all LTC695x parts */
    for (array_loc=0; array_loc<5; array_loc++) {
    LTC695x_lookuptbl_write(array_loc,LTC695x_Site_list,LTC695x_lkup_tbl);
    } /* end of for loop - array_loc... */

    /* STEP 3: SYNCRONIZE OUTPUT STAGES and 2 by toggling the Stage 1 LTC6953 SSRQ bit in addr 0x0B */
    Serial.println(F("\n\nInitial Registers Loaded: "));
    Serial.println(F("Press <ENTER> to sync (EZSync) STAGE 1&2 reference outputs: "));
    user_command = read_int(); //! Reads the user command

    changeDC2430site(0); // switch DC2430 site
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SSRQ, 1);
    delay(1); // min 1ms delay for SSRQ HIGH pulse
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SSRQ, 0);
    delay(1); // min 1ms delay for SSRQ LOW pulse

    /* OPTIONAL STEP 4a1: ADJUST STAGE 1 ADEL values if desired, this lines up the reference edges at the STAGE 2 inputs,
    will need to resync as this can cause the follower input to glitch */
    /* OPTIONAL STEP 4a2: ADJUST STAGE 2 ADEL values if desired, this lines up the reference edges at the STAGE 3 inputs,
    no resync necessary */


    /* **** PARALLEL SYNC STAGE 3. THIS IS DONE BY STEPS 5-7
    5) this is done by enabled SRQMD=1, which will retime STAGE 1 & STAGE 2 PASS-THRU OUTPUTS to
    the input reference signal
    6) disabled SQEN for on ALL STAGE 1 and 2 CLOCK OUTPUTS
    7) Toggle STAGE 1 SSRQ BIT, this will ParallelSync the STAGE 3 outputs */
    Serial.println(F("\nStage 2 REFERENCES synchronized: "));
    Serial.println(F("Press <ENTER> to sync (ParallelSync) STAGE 3 clock outputs: "));
    user_command = read_int(); //! Reads the user command

    for (array_loc=0; array_loc<=2; array_loc++) {
    changeDC2430site(LTC695x_Site_list[array_loc]); // switch DC2430 site
    // STEP 5. this is done by enabled SRQMD=1, which will retime STAGE 1 & STAGE 2 PASS-THRU OUTPUTS to the input reference signal
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SRQMD, 1);
    // STEP 6. disabled SQEN for on ALL STAGE 1 and 2 CLOCK OUTPUTS
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SRQEN4, 0);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SRQEN8, 0);
    } /* end of for loop - array_loc... */
    // STEP 7. Toggle STAGE 1 SSRQ BIT, this will ParallelSync the STAGE 3 outputs
    changeDC2430site(0); // switch DC2430 site
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SSRQ, 1);
    delay(1); // min 1ms delay for SSRQ HIGH pulse. ***
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SSRQ, 0);
    delay(1); // min 1ms delay for SSRQ LOW pulse

    /* **** SEND SYSREF FROM STAGE 3. THIS IS DONE BY STEPS 8-10
    8) Power up STAGE 3 SYSREF outputs (PDx=0)
    9) Set all STAGE 3 LTC6952 SRQMD=1
    10) Toggle STAGE 1 SSRQ BIT, this will ParallelSync the STAGE 3 outputs */
    Serial.println(F("\nStage 3 OUTPUTS synchronized: "));
    Serial.println(F("Press <ENTER> to send Stage 3 SYSREF PULSES: "));
    user_command = read_int(); //! Reads the user command

    for (array_loc=3; array_loc<=4; array_loc++) {
    changeDC2430site(LTC695x_Site_list[array_loc]); // switch DC2430 site
    // STEP 8. Power up STAGE 3 SYSREF outputs (PDx=0)
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD0, 0);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD2, 0);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD4, 0);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD7, 0);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD9, 0);

    // STEP 9. Set all STAGE 3 LTC6952 SRQMD=1
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SRQMD, 1);
    } /* end of for loop - array_loc... */
    delay(1); // delay min of 50us for SYSREF pins to power up.

    // STEP 10. Toggle STAGE 1 SSRQ BIT, this will ParallelSync the STAGE 3 outputs
    changeDC2430site(0); // switch DC2430 site
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SSRQ, 1);
    delay(1); // min 1ms delay for SSRQ LOW pulse
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SSRQ, 0);
    delay(1); // min 1ms delay for SSRQ LOW pulse

    // OPTIONAL STEP 11. Power down STAGE 3 SYSREF outputs (PDx=2)
    Serial.println(F("\nSYSREF PULSES SENT: "));
    Serial.println(F("Press <ENTER> to power down SYSREF outputs and set SRQMD=0: "));
    user_command = read_int(); //! Reads the user command

    for (array_loc=3; array_loc<=4; array_loc++) {
    changeDC2430site(LTC695x_Site_list[array_loc]); // switch DC2430 site
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD0, 2);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD2, 2);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD4, 2);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD7, 2);
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_PD9, 2);
    } /* end of for loop - array_loc... */

    // STEP 12. Set SRQMD=0 to save Power ~300mW per device
    for (array_loc=0; array_loc<5; array_loc++) {
    changeDC2430site(LTC695x_Site_list[array_loc]); // switch DC2430 site
    set_LTC6952_SPI_FIELD(QUIKEVAL_CS, LTC695x_SRQMD, 0); /* resets all devices every run */
    } /* end of for loop - array_loc... */

    } /* end of if DC2430_Bin == 1 */
    }

  • Hi Chris!

    I need technical support about LTC6952 and LTC6953 “ParallelSync Multi-Chip Synchronization with Request Passthrough” three stage configuration (according to LTC6952 datasheet page 76). I would like to know if is it possible to connect in a daisy-chain configuration those chips placed on different boards as shown below:

    Can I try this configuration using LTC6952Wizard, DC2026 board, DC2430A exapansion board, 3 x DC2610A boards and 3 x DC2609A boards? Are there just available some .6952set files in LTC6952Wizard tool to try this configuration? What's the maximum number of different boards in daisy-chain configuration to ensure a good synchronization? Thank you so much.

    Best Regards

    Antonio

  • Hey Antonio,

    You can try this configuration with the DC2430A.  

    Before getting into detailed of a discussion, is this a JESD204B or JESD204C clock application that requires a SYSREF signal?

    Chris

  • My application is a JESD204B clock application that requires a SYSREF signal. Every LTC6952 chip in each board I showed you supplys Device Clock and SYSREF to an FPGA and to a Fast ADC that communicate through a JESD204B link.

  • And so I want to synchronize every LTC6952 output clock generation to make a synchronized distributed system connected in a daisy-chain configuration, like that I showed you. But I would like to try that before I design my board.

  • Antonio,

    In this daisy chain configuration is it limited to 3 boards deep as shown (1 master and 2 slaves) or could this in theory add several more slave stages? If so, how many?

    Also, in the diagram above you show a 100MHz reference.  I'm assuming you only want to send the 100MHz reference and EZS_SRQ to the other boards.  however, are there any other divided frequencies coming off of the LTC6953s that are not shown?  I'm trying to figure out if all the non-EZS_SRQ signals are just /1s or if there are any other divided frequencies coming from the LTC6953s.

    I've done a couple configs somewhat similar to this and little details can affect the setup some.  So I want to make sure I give you the correct pointers...

    Thanks

    Chris

  • Chris,

    in my configuration I would like to connect a maximum of 10 slaves to a master. I don't care how long it takes because I suppose this multi stage synchronization is only in a startup phase. Is it true? Or do I must periodically refresh it?

    A single board can work standalone if not connected in a distributed system.

    I'm going to show you the real configuration I would like to do:

    In general do you confirm me that I can try this with those evaluation boards (LTC6952Wizard, DC2026 board, DC2430A exapansion board, n x DC2610A boards and n x DC2609A boards)? Am I evaluating the right configuration to my project scope?

    Thank you.

    Antonio

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.