Hi,
We will be designing a custom based board based on ADRV9008-2 with Xilinx FPGA. With regard to that out of AD9528 or HMC7044 which one will be providing better performance
Regards,
Sudarshan
AD9528
Recommended for New Designs
The AD9528 is a two-stage PLL with an integrated JESD204B/JESD204C SYSREF generator for multiple device synchronization. The first stage phase-locked loop...
Datasheet
AD9528 on Analog.com
HMC7044
Recommended for New Designs
The HMC7044 is a high performance, dual-loop, integer-N jitter attenuator capable of performing reference selection and generation of ultralow phase noise...
Datasheet
HMC7044 on Analog.com
ADRV9008-2
Recommended for New Designs
The ADRV9008-2 is a highly integrated, RF agile transmit subsystem offering dual channel transmitters, observation path receiver, integrated synthesizers...
Datasheet
ADRV9008-2 on Analog.com
Hi,
We will be designing a custom based board based on ADRV9008-2 with Xilinx FPGA. With regard to that out of AD9528 or HMC7044 which one will be providing better performance
Regards,
Sudarshan
the same question, but in board with 2x ADRV9026 + Kintex 7
HI,
the AD9528 can be used with a Crystek 122.88 MHz VCXO ( CVHD-950-122.880, the one it populates as Y2 on the AD9528 evaluation board) to provide DEVCLK to ADRV9026. Keep RF PLL BW to at least 200 kHz, so EVM levels 5 to 7 dB lower than -40 dB can be obtained.
The AD9528 is used on the ADRV9008 evaluation board, so the AD9528 should provide the right DEVCLK to the ADRV9008 as well.
I do not support HMC7044, so I cannot state anything about it.
These questions should be posted on the ADRV community websites, so the apps engineers supporting the ADRV chips are able to provide their inputs.
Petre
HI,
the AD9528 can be used with a Crystek 122.88 MHz VCXO ( CVHD-950-122.880, the one it populates as Y2 on the AD9528 evaluation board) to provide DEVCLK to ADRV9026. Keep RF PLL BW to at least 200 kHz, so EVM levels 5 to 7 dB lower than -40 dB can be obtained.
The AD9528 is used on the ADRV9008 evaluation board, so the AD9528 should provide the right DEVCLK to the ADRV9008 as well.
I do not support HMC7044, so I cannot state anything about it.
These questions should be posted on the ADRV community websites, so the apps engineers supporting the ADRV chips are able to provide their inputs.
Petre