Post Go back to editing

LTC6908 Compatibility with Various Converters

Thread Summary

The user inquired about synchronizing LT3796, LTC3126, and LTC3622 converters with an LTC6908 at 560 kHz with spread spectrum. The final answer confirms compatibility but notes that narrow closed-loop bandwidth in the converters may affect tracking of the spread spectrum modulation, potentially increasing output ripple. The LTC6908 offers three modulation rate settings to accommodate various switchers.
AI Generated Content

I am investigating using an LTC6908 in an application with multiple power converters. In this application, it would run at a nominal frequency of 560 kHz (504 kHz to 616 kHz with spreading). I am hoping to confirm that all the converters that will be sync'd to it are able to do so -- in particular, I'm concerned about behavior with a spread spectrum clock into a converter that might, for example, have an undocumented PLL. The following converters are used in the design:

LT3796
LTC3126
LTC3622

Can you confirm that all of these devices are expected to be able to synchronize to an LTC6908?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.