LTC 6955 some problem

I   use the LTC6955  as clock  distributer , im my circuit diagram, have seven ad9266s. the board work at  atmoshpere temperature is 125℃ at least four hours,(satisfy the target temperature only three types of chips). In the LTC6955 document, only supply single-ended sine wave signal  or Differential signal input, AD9266 work on 40MHZ  frequency(the ltc6955 clock source at 40Mhz), 

I'm sensitive the CLOCK JITTER and  work temperature and ADC sampling  Time synchronization,

    my question is : the input clock  can use single-ended square wave clock  as the input clock?,if can ,can give me a circuit diagram,

Best Regards

 Crusadelee



errors
[edited by: crusadelee at 10:56 AM (GMT 0) on 21 Nov 2019]
Parents Reply Children