I use the LTC6955 as clock distributer , im my circuit diagram, have seven ad9266s. the board work at atmoshpere temperature is 125℃ at least four hours,(satisfy the target temperature only three types of chips). In the LTC6955 document, only supply single-ended sine wave signal or Differential signal input, AD9266 work on 40MHZ frequency(the ltc6955 clock source at 40Mhz),
I'm sensitive the CLOCK JITTER and work temperature and ADC sampling Time synchronization,
my question is : the input clock can use single-ended square wave clock as the input clock?,if can ,can give me a circuit diagram,
Best Regards
Crusadelee
errors
[edited by: crusadelee at 10:56 AM (GMT 0) on 21 Nov 2019]