No output of AD9545 OUT1A

Hi 

I build the configuration of AD9545  by the ACE and dump the memory and apply *.txt in FBGA.

In our board,the OUT0A and OUT0B could generate 125MHz and 156.25MHz signal as we wish.

But there is no signal (30.72MHz) in OUT1A.

Could you help to check if the configuration is correct?

REF A=125 MHz

REF AA = 156.25 MHz

REF B = 30.72 MHz

REF BB = 1 Hz (from the GPS)

Abao



upload the ACE config pic
[edited by: ALin773 at 2:22 AM (GMT 0) on 29 Oct 2019]
Parents
  • +1
    •  Analog Employees 
    on Oct 29, 2019 6:00 PM 11 months ago

    HI,

    Please send me your cso file you obtained with ACE to check it.

    There are multiple steps you have to make sure you take after you obtain a configuration file from ACE. Please make sure you follow them. They are outlined in Initialization sequence section at page 160 in rev B data sheet.

    Make also sure the driver of OUT1A (that is HCSL or CML) matches the hardware.

    Make sure you generated a SYNC operation.

    There may be other reasons, but I need to see the cso file first.

    Petre

Reply
  • +1
    •  Analog Employees 
    on Oct 29, 2019 6:00 PM 11 months ago

    HI,

    Please send me your cso file you obtained with ACE to check it.

    There are multiple steps you have to make sure you take after you obtain a configuration file from ACE. Please make sure you follow them. They are outlined in Initialization sequence section at page 160 in rev B data sheet.

    Make also sure the driver of OUT1A (that is HCSL or CML) matches the hardware.

    Make sure you generated a SYNC operation.

    There may be other reasons, but I need to see the cso file first.

    Petre

Children