No output of AD9545 OUT1A

Hi 

I build the configuration of AD9545  by the ACE and dump the memory and apply *.txt in FBGA.

In our board,the OUT0A and OUT0B could generate 125MHz and 156.25MHz signal as we wish.

But there is no signal (30.72MHz) in OUT1A.

Could you help to check if the configuration is correct?

REF A=125 MHz

REF AA = 156.25 MHz

REF B = 30.72 MHz

REF BB = 1 Hz (from the GPS)

Abao



upload the ACE config pic
[edited by: ALin773 at 2:22 AM (GMT 0) on 29 Oct 2019]