ret=ad9518_spi_write(dev, 0x0000, 0xbd); //set SPI port miso
ret=ad9518_spi_write(dev, 0x0232, 0x01);
ret=ad9518_spi_write(dev, 0x0000, 0x99);
ret=ad9518_spi_write(dev, 0x0232, 0x01);
ret=ad9518_spi_write(dev,0x0010,0xCC); //8bit low for up frequency
ret=ad9518_spi_write(dev,0x0011,0x05);
ret=ad9518_spi_write(dev,0x0012,0x00);
ret=ad9518_spi_write(dev,0x0013,0x00);
ret=ad9518_spi_write(dev,0x0014,0x18);
ret=ad9518_spi_write(dev,0x0015,0x00);
ret=ad9518_spi_write(dev,0x0016,0x06);
ret=ad9518_spi_write(dev,0x0017,0x10); //status is P divoder output
//ret=ad9518_spi_write(dev,0x0018,0x60);
ret=ad9518_spi_write(dev,0x0019,0x00);
ret=ad9518_spi_write(dev,0x001A,0x00); //DLD
//ret=ad9518_spi_write(dev,0x001B,0x60); //refmon 0x62 ref2 0x61 ref1
ret=ad9518_spi_write(dev,0x001B,0xE1); //1 for Ref1,2 for ref2 8bit=VCO monitored
ret=ad9518_spi_write(dev,0x001C,0x06); //0x46 ref2 0x06 ref1
ret=ad9518_spi_write(dev,0x001D,0x00);
ret=ad9518_spi_write(dev,0x001E,0x00);
ret=ad9518_spi_write(dev,0x00F0,0x0A);
ret=ad9518_spi_write(dev,0x00F1,0x0A);
ret=ad9518_spi_write(dev,0x00F2,0x08);
ret=ad9518_spi_write(dev,0x00F3,0x08);
ret=ad9518_spi_write(dev,0x00F4,0x0A);
ret=ad9518_spi_write(dev,0x00F5,0x0A);
ret=ad9518_spi_write(dev,0x0190,0x00);
ret=ad9518_spi_write(dev,0x0191,0x80);
ret=ad9518_spi_write(dev,0x0192,0x00);
ret=ad9518_spi_write(dev,0x0193,0xBB);
ret=ad9518_spi_write(dev,0x0194,0x80);
ret=ad9518_spi_write(dev,0x0195,0x00);
ret=ad9518_spi_write(dev,0x0196,0x00);
ret=ad9518_spi_write(dev,0x0197,0x80);
ret=ad9518_spi_write(dev,0x0198,0x00);
ret=ad9518_spi_write(dev,0x01E0,0x04);
ret=ad9518_spi_write(dev,0x01E1,0x02);
ret=ad9518_spi_write(dev,0x0230,0x00);//04 no sync
ret=ad9518_spi_write(dev,0x0232,0x01);
//VCO calibration
ret=ad9518_spi_write(dev,0x0018,0x60); //VCO calibration low
ret=ad9518_spi_write(dev,0x0232,0x01);
ret=ad9518_spi_write(dev,0x0018,0x61); //VCO calibration begin
ret=ad9518_spi_write(dev, 0x0232, 0x01);
mdelay(50);
ret=ad9518_spi_write(dev,0x001D,0x0D);
ret=ad9518_spi_write(dev, 0x0232, 0x01);//enable hold over
ret=ad9518_spi_write(dev,0x0017,0x04);//status is N divoder output
ret=ad9518_spi_write(dev, 0x0232, 0x01);
best wishes !