About ad9523 pll1_out and vcxo

Hi, I have question about ad9523's 72th pin.

I'm using VCXO which center frequency is 125MHz.

The problem is that when I tried to do get a signal on pin Pll1_out, the signal doesn't come out anything. It's just look like ground.

I powered up the PLL1 and divider was just 1.0, and I used ad9523 evaluation software to match the register.( I used the FPGA to wirte SPI, this worked well. I verify it with SDO pin.)

The reason I am guessing is that my AD9523 doesn't read the VCXO's signal. So is there any way or spi register that I have to modify? or do I need to give signal to other pin?

sorry for short English.

Taehyung.

Parents
  • 0
    •  Analog Employees 
    on May 24, 2019 2:30 PM

    HI Taehyung,

    I'm sorry for the delay in getting back to you.

    to get the VCXO output at pin PLL1OUT, you need to enable the PLL1 output driver by setting bit 7 in register 0x1BB to 1. The best way is to use an evaluation board, obtain a configuration file from it based on your choices, and see the registers setup from this file.

    Petre

Reply
  • 0
    •  Analog Employees 
    on May 24, 2019 2:30 PM

    HI Taehyung,

    I'm sorry for the delay in getting back to you.

    to get the VCXO output at pin PLL1OUT, you need to enable the PLL1 output driver by setting bit 7 in register 0x1BB to 1. The best way is to use an evaluation board, obtain a configuration file from it based on your choices, and see the registers setup from this file.

    Petre

Children
No Data