The subband of HMC835 is obtained by reading back, and then the register configuration in manual calibration mode is used, Reg 0Ah = 00084350h; Reg 15h = 0F4BE3A8h; the initialization frequency is 2150MHz, but it has been out of lock. How to configure the register in manual calibration mode? Register configuration is as follows:
Reg 00h=00002000h;
Reg 01h=00000308h;
Reg 02h=00000110h;
Reg 05h=00000028h;
Reg 06h=030F0A30h;
Reg 07h=200A4438h;
Reg 08h=41BFFF40h;
Reg 09h=54726448h;
Reg 0Ah=00084350h;
Reg 0Bh=07C02158h;
Reg 0Ch=00000060h;
Reg 0Fh=00000178h;
Reg 14h=000220A0h;
Reg 15h=0F4BE3A8h;
Reg 16h=0006C1B0h;
Reg 17h=0001ABB8h;
Reg 18h=0054C1C0h;
Reg 19h=000AAAC8h;
Reg 1Ah=B29D0BD0h;
Reg 03h=00002B18h;
Reg 04h=00000020h;