Hi, I am wondering if there are any plans to make a LTSpice model for the comparator LTC6957. This comparator would really benefit from a good model, due to its unusual input characteristics.
Thanks!
Colin
LTC6955
Last Time Buy
The LTC6955 is a high performance, ultralow jitter,
fanout clock buffer with eleven outputs. Its 4-pin parallel
control port allows for multiple output...
Datasheet
LTC6955 on Analog.com
LTC6954
Last Time Buy
The LTC6954 is a family of very low phase noise clock distribution parts. Each part has three outputs and each output has an individually programmable...
LTC6954 on Analog.com
Hi, I am wondering if there are any plans to make a LTSpice model for the comparator LTC6957. This comparator would really benefit from a good model, due to its unusual input characteristics.
Thanks!
Colin
The LTC6957, LTC6954 and LTC6955 datasheet have lots of tested/verified input schematics that can be used for a variety of input signal types. The LTC6957 input is very similar to the LTC6954 and LTC6955 so all these apply. The LTC6954 and LTC6955 datasheets have more input schematics than the LTC6957 as these were 2nd and 3rd generation datasheets. No LTSpice model.
The LTC6957, LTC6954 and LTC6955 datasheet have lots of tested/verified input schematics that can be used for a variety of input signal types. The LTC6957 input is very similar to the LTC6954 and LTC6955 so all these apply. The LTC6954 and LTC6955 datasheets have more input schematics than the LTC6957 as these were 2nd and 3rd generation datasheets. No LTSpice model.