Post Go back to editing

AD9528 jitter question

Thread Summary

The user inquires about the jitter performance of the AD9528 clock generator in an ultrasound system. In Buffer Mode, the total RMS jitter for the AFE ADC clocks is calculated as 180.3 fs RMS. In PLL Mode, the absolute jitter is 179 fs, and the crystal jitter does not need to be considered. The user is advised to separate analog and digital grounds and connect them at one point for the AFE ADC. The engineer recommends reviewing Analog Devices' PLL and jitter tutorials for further guidance on CWx16 clock jitter selection and layout.
AI Generated Content

Hi there,

We are using AD9528 as our clock generator in ulrasound system.

Basic topology is:  Crystal(200MHZ, 100fs jitter rms) ---> AD9528 ----> Clock Fanout Buffer IC(ADCLK854,54fs rms) ----> AFE ADC(may use AD9276).

All LVDS clocks.

Some questions about Jitters of AD9528. 

1. If we use Buffer Mode, Output Additive Jitter is about 140fs. so total rms jitter for AFE ADC clocks should be roots.quare(100*100+140*140+54*54) = 180.3fs rms. Is my perception correct?

2. If we use PLL Mode, OUTPUT 【Absolute】 Time Jitter is about 179fs. For the "Absolut jitter", does is mean , there is no need to consider jitter of Crystal ? Not sure about this.

3. For AFE ADC GND layout, is it necessray to seperate Analog GND and Digital GND, and connect them at one point? Or could we use one complete GND plane? 

4. Any suggestions on CWx16 clocks jitters selection? Also, guidance on layout and routing about CW siganl is appreciated

Thanks very much!

XY

Parents
  • Hi, any ADI guys could help on this?  Thanks.

  • Chapter 9 Hardware Design Techniques F.pdfHi XY,

    let me respond to your questions:

    If we use Buffer Mode, Output Additive Jitter is about 140fs. so total rms jitter for AFE ADC clocks should be roots.quare(100*100+140*140+54*54) = 180.3fs rms. Is my perception correct?

    Yes. It seems you are focusing on using LVDS outputs and are concerned only about the12kHz to 20 MHz frequencies. Please note that these numbers were obtained using an external 122.88 MHz source driving VCXO inputs, which may not be your case. Then, please pay attention to the slew rate of the inputs. The figure 19, page 21 in the data sheet shows the rms jitter increases very fast for slew rates below 0.25V/ns:

    2. If we use PLL Mode, OUTPUT 【Absolute】 Time Jitter is about 179fs. For the "Absolut jitter", does is mean , there is no need to consider jitter of Crystal ? Not sure about this.

    Yes, the absolute jitter includes all the source noises that come into the chip, not only the noise created by the chip (which is the additive noise).

    3. For AFE ADC GND layout, is it necessray to seperate Analog GND and Digital GND, and connect them at one point? Or could we use one complete GND plane? 

    This is what the theory says. Please take a look at the attached Hardware Design Techniques chapter (page 9.32, figure 9.22)  of the Data Conversion Handbook that you can find here:

    https://www.analog.com/en/education/education-library/data-conversion-handbook.html

    But the easiest approach is to copy the layout of the AD9276 from its evaluation board. I see an evaluation board manual (UG-016) that contains the schematic and the layout. Gerber files are provided on its webpage.

    1. Any suggestions on CWx16 clocks jitters selection? Also, guidance on layout and routing about CW siganl is appreciated

    Please note I do not know the AD9276, but I suggest following the layout of the evaluation board.

    Best regards

    Petre

Reply
  • Chapter 9 Hardware Design Techniques F.pdfHi XY,

    let me respond to your questions:

    If we use Buffer Mode, Output Additive Jitter is about 140fs. so total rms jitter for AFE ADC clocks should be roots.quare(100*100+140*140+54*54) = 180.3fs rms. Is my perception correct?

    Yes. It seems you are focusing on using LVDS outputs and are concerned only about the12kHz to 20 MHz frequencies. Please note that these numbers were obtained using an external 122.88 MHz source driving VCXO inputs, which may not be your case. Then, please pay attention to the slew rate of the inputs. The figure 19, page 21 in the data sheet shows the rms jitter increases very fast for slew rates below 0.25V/ns:

    2. If we use PLL Mode, OUTPUT 【Absolute】 Time Jitter is about 179fs. For the "Absolut jitter", does is mean , there is no need to consider jitter of Crystal ? Not sure about this.

    Yes, the absolute jitter includes all the source noises that come into the chip, not only the noise created by the chip (which is the additive noise).

    3. For AFE ADC GND layout, is it necessray to seperate Analog GND and Digital GND, and connect them at one point? Or could we use one complete GND plane? 

    This is what the theory says. Please take a look at the attached Hardware Design Techniques chapter (page 9.32, figure 9.22)  of the Data Conversion Handbook that you can find here:

    https://www.analog.com/en/education/education-library/data-conversion-handbook.html

    But the easiest approach is to copy the layout of the AD9276 from its evaluation board. I see an evaluation board manual (UG-016) that contains the schematic and the layout. Gerber files are provided on its webpage.

    1. Any suggestions on CWx16 clocks jitters selection? Also, guidance on layout and routing about CW siganl is appreciated

    Please note I do not know the AD9276, but I suggest following the layout of the evaluation board.

    Best regards

    Petre

Children