HMC1033 Minimal Configuration

Hello,

is there a minimal configuration available for the HMC1033? I'm designing a testbed for a board containing this IC and fine tuning will be done later by different people. For simple liveness test I'd link to have a simple configuration that takes a 10MHz input clock (CMOS into XREF) and outputs a clock in the order of magnitude of 100MHz. I do not care about performance at this point. I already verified that the SPI interface is operational an I can read and write registers.

Unfortunately the available simulation tools are not very helpful and the only discussion on this message board about this part appears to be in Chinese. Any help is appreciated,

Thank you!