Can you compare the advantages/disadvantages of the HM704x clock family vs the LTC695x family? They seem like very similar parts.
ADI offers the two lowest jitter JESD204B/C multi-output clock generation devices on the market in the <4.5GHz frequency range. While these devices are very similar in some respects, there are some fairly…
I'd like to ask you a question that whether the LTC6952's output can be the input of AD9528's VCO?
Yes, if you AC couple the signal, as The LTC6952's output common mode is different than the AD9528 VCXO pin's input common mode requirement.
I'm curious why this combination is of interest. Are you trying to take advantage of the AD9528's jitter clean-up loop (PLL1) or some other feature? The reason I ask, is I am trying to figure out if you have the best combination of parts for what you are trying to achieve.
Thanks for your answer! The reason why I pick LTC6952 is that it can operate in very high frequency. As for AD9528,is I want to use AD9528 for AD9371. In the meanwhile,I want to make all clocks in my system operate from a same sourse.So,I use LTC6952 as the sourse of AD9528.