Hello,
I have a few questions regarding signal integrity.
1. I'm planning on using the LT6957-3 part in a design for a diode driver. The diode driver is the LMG1020 and is driven directly from the LTC6957-3 output. The length of the trace is roughly 0.6" (inches). The rise time for the 6957-3 is 320pS. We are trying to send a 1-2nS pulse through this part (powered with a Vcc=3.3V). Since this output is CMOS logic how do you properly handle this 0.6" track length regarding terminations etc....for best signal integrity?
2. With this length is the signal degradation a large issue?
3. Is there any way to check this in LTspice?
4. Can you convert an IBIS model to a spice model for use in LTspice?
4a. if so - how and/or where is documentation explaining this?
Thank you for any response/advice!