I use ltc6953,Config all channel for Mode 0,Srqen set 0,ddely adely also set 0,as datasheet it is free running,only set divider,but no outputs,register 0xb set 0,during config ltc6953,I set sd_ to be 1 all,does it need to config sync operation?anyone can give me a free running config for me,thanks.
And register 0 has field vcook and vcook_,when sd_ set 1,vcook is 1,vcook_ is 0,otherwise vcook is 0,vcook_ is 1;when sd_ is 1,even if no signal in ltc6953's clk in port,vcook also is 1,what means does field vcook?