Article AD9523-1: Can I bypass PLL1 and only use the PLL2?

Question

Can I can bypass the PLL1 in AD9523-1 and input a ref clock at the OSC pins
directly?
In the datasheet, I don't find any register to disable the PLL1, so I am not
sure it is OK to bypass it.

Answer

Yes the AD9523, AD9523-1, and AD9524 can all be configured as a single loop
device and offer a low power clock generator distribution solution.

To use only the second loop PLL(2) the input reference to the PLL would be the
OSC_IN input(s) either configured as single-ended CMOS or differential. There
is a power down bit for PLL1 but this can NOT be used because it will also
power down the OSC_IN input receivers. To save power individual PLL1 blocks
can be powered down: REFA and REF input receivers (reg h01A), Charge pump
current set to 0 and tristate (reg h018 and h019), and Zero Delay receiver (reg
h01B).

To use only the first loop PLL(1) Outputs 0, 1, 2, 3 on the AD9523 and AD9523-1
can be configured to output PLL1. The AD9524 Outputs 0 and 1 can be used to
output PLL1. To reduce power disable: power down unused output channels,
Charge pump current set to 0 and tristate (reg h0F0 and h0F2), VCO divider (reg
h0F4), and Zero Delay receiver (reg h01B).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.