Article AD9510: Outputs not in Phase

Question

for evalution board AD9510, on the CLK1 input 1001.6 MHz, ratio 8 for output5
and output6 equal 125.2 MHz. For on/off, on/off ext. clock (1001.6 MHz) have
shift phase between output5 and output6 equal 90 or 180 or 270 or 0 degree.

Answer

It is necessary to do a register update AFTER each write to the Soft Sync bit.
That is, it is necessary to load the Soft Sync bit by updating the registers
with the 0x5A=1.

Here is my recommended sequence:

1) write all of the desired parameters for the AD9510
2) write 0x5A=1 (update internal registers)
3) write 0x58
4) write 0x5A=1 (update internal registers)
5) write 0x58
6) write 0x5A=1 (update internal registers)

Try this and see if it fixes the problem.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.