Article What is the duty cycle of the DS3231/2/4 32kHz Output?

The output will be a square wave with a duty cycle of anywhere between 31% and 69%. This duty cycle depends on when the edges of the crystal's oscillation (the crystal being mounted in the package area between pins 7-10 and 11-14) cross the internal 'detect' threshold (typically 0.7V, but since this is an internal function it is not specified in the datasheet).  The closer the crystal's oscillations are to the 'detect' threshold, the closer to 50% duty cycle you can expect the 32kHz output. For timekeeping in this IC, we are only counting edges of the 32kHz signal, so duty cycle is not a concern for our timekeeping design.  But for those expecting to use the 32kHz output, you can expect anywhere from 31% to 69% duty cycle.  There is no way to adjust this duty cycle.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.