Q: What is the status of the DS1683EVKit and EVKit data sheet? Several places on the Maxim site mention this kit but the DS1683 device data sheet and the Maxim site provide no links for the kit. A:
There…
Q: Operating temperature range for DS1683 is -40 ⁰C to 85 ⁰C but the Programming temp range specified is 0 ⁰C to 70 ⁰C . Why are they different?
A: The Programming Temperature is the range under which…
Q: In the DC Electrical Characteristics there are entries for Active Supply Current (ICCA) and EEPROM Write Current (IEE). Is the EEPROM write current additional to the supply current? What is the maximum…
The ETC register is a four-byte register. In order to read the ETC register properly, users should follow the reading procedure at following.
Start -> Slave address write byte (D6h) -> Slave Ack ->…
Below are some of the programming differences between DS1682/DS1683. In general the devices are very similar, but there are some potential functional pitfalls customers may see when switching between the…
To prevent interruption of the EEPROM write cycle, there must not be any I2C commands issued during the 20ms EEPROM Write Time (tW). If you do not wait the full 20ms after each write, then there is a risk…
The 0xFFFF failures may be attributed to a truncated tW time. To prevent interruption of the EEPROM write cycle, there must not be any I2C commands issued during the 20ms EEPROM Write Time (tW). If you…
If the EEPROM write is interrupted, it could cause a 1's value. The first step in the EEPROM write cycle is to set the registers to all 1's, then the second stage writes the new value. If the EEPROM write…