I am try to get a thermocouple by AD7124-4 application again.

Hello

I met AD7124 IC two years ago.

I knew great works well. I made 10 boards on same circuit as bellow.

when I turn on the board and check a coldjunction temperature(RT1), the 5 borads temperature is different.

the 5 boards are about 24 degree and the other boards are 30 degree. the part is used same.

what do i do wrong? 

my code is like this:

1) reset data send ( 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff)

2) channel-0 setting ( 0x09, 0x10, 0xA6)      // AINP=AIN5,     AINM= AIN6

3) config-0 setting ( 0x19, 0x01, 0xEF)      // unipolar, ref_bufp

4) filter-0 setting ( 0x21, 0xE6, 0x07, 0xFF)

5) IOUT setting (0x03, 0x00, 0x12, 0x0B)

6) when i read, (0x01, 0x01, 0x84); // ADC controll setting

                         (0x42, 0x00, 0x00, 0x00, 0x00) // read

 i send number 6) messages on period.

please, check my setting codes and help me.

thanks for reading.

Parents
No Data
Reply
  • Hi Brandon

    I understand your disclaimer about Analog Devices.

    A problem is that my english skill is poor. So I know misunderstand of 7124 datasheet.

    I just reference your software source codes.

    My problem is I cant control two channel operations.

    I use the NTC for coldjunction temperature and Thermocouple for Hot point temperature. So I have to use two channels of 7124-4 IC.

    I just want to how to channel settings for two resources through your C language source codes.

    There is no sources in the link.

    can you show me how to send the packet in the CN0376 devices?

    I am using the 7124-4 like this flow on my code:

    RESET for 7124-4

    setting for NTC at channel-0

    data reading for NTC

    after 1 sec

    RESET for 7124-4

    setting for Thermocouple at channel-0

    data reading for Thermocouple

    go back to first step.

    But I want to that like this flow:

    RESET for 7124-4

    setting for NTC at channel-0

    setting for Thermocouple at channel-1

    data reading for NTC

    data reading for Thermocouple

    data reading for NTC

    data reading for Thermocouple

    data reading for NTC

    data reading for Thermocouple

    My thermocouple setting is not right, so thermocouple data is not useful..

    1st question:

    If there is ADICUP360 codes for CN0376 devices, share for me. I will just check the packet for NTC and Thermocouple.

     

    2nd question:

    Is it ok when I reset the 7124-4 IC frequently ? actually, I cant set two channels, I do reset operation for channel-0.

    thank you for reading. thank you very much.

Children
No Data