cn-0209

Hi,

      I need to design a universal analog input module .I have referred to CN-0209.But I could not understand the purpose of ADG442 used in the circuit.Can I get help?

Regards,

Divya

Parents
  • Hi,

       In my project,I require atleast two UART and two CAN interfaces to enable the communication of the Analog Input Module  with the CPU .So a controller having two UART and two CAN interfaces is necessary ,right?So can AduCM361 be used here?Is ADSP-CM402F/CM403F/CM407F/CM408F suitable here?Please help me regarding the microcontroller selection.

    Regards,

    Divya

Reply
  • Hi,

       In my project,I require atleast two UART and two CAN interfaces to enable the communication of the Analog Input Module  with the CPU .So a controller having two UART and two CAN interfaces is necessary ,right?So can AduCM361 be used here?Is ADSP-CM402F/CM403F/CM407F/CM408F suitable here?Please help me regarding the microcontroller selection.

    Regards,

    Divya

Children
No Data