Hello,
I want to make a precision 40mA low side current sink that can work with 5V to 300 Volts maximum, for use in a pro audio amplifier. Any voltage up to 100V is also available to power the solution circuit.
Has to work -40 C to + 85 C
Gary
Hello,
I want to make a precision 40mA low side current sink that can work with 5V to 300 Volts maximum, for use in a pro audio amplifier. Any voltage up to 100V is also available to power the solution circuit.
Has to work -40 C to + 85 C
Gary
Another option would be to use two MJE340's in a darlington pair configuration. This would increase HFE and decrease bias current errors. Alternatively, a high voltage MOSFET would also work. The amplifier you have looks fine. I'd go with an LT1027 or LT6657 for the reference.
Another option would be to use two MJE340's in a darlington pair configuration. This would increase HFE and decrease bias current errors. Alternatively, a high voltage MOSFET would also work. The amplifier you have looks fine. I'd go with an LT1027 or LT6657 for the reference.