Post Go back to editing

CN-0507 on the ADICUP3029

 Hi,

 I am testing the EVAL-CN0507-ARDZ demo board together with the EVAL-ADICUP3029 board and problems have arisen:
_ Is the firmware to be used cn0507-vna-app-firmware-20033101.hex?
_After installing the firmware above the board generates a virtual COM which in my case was COM6 but the ADI VNA APP software cannot recognize the port! Why?
_ The EVAL-CN0507-ARDZ board is consuming 1A from the 6Vdc source and the components heat up! Does this really happen?

Regards

Parents Reply Children
No Data