Hi,
I would like to modify the CN-0359 RTD coding. Resistance to Temperature. I found the following detail in "CN0359-SourceCode-RevA" folder (ADC.cpp file)
Could ADI have any detail for the formula above? Such parameter Radc, 1V, 500nA/V.....
In CN-0359 datasheet, the following is the formula of RTD. It look different from the Coding
Besides, if I follow the formula in ADC.cpp, it does not match the following in function - on_adc1(int argc, char *argv[]) :
The value is different from the RTD equation as well
Appreciate if you can advise further how RTD code is working.
Thank for your help in advance.
Mark.