IEPE Data Acquisition Board (EVAL-CN0540-ARDZ)

I am designing a vibration monitoring circuit that needs to gather vibration data from a vibration table in 2 dimensions. I am wanting to use an IEPE sensor with 50 g range, 100mv/g sensitivity, and a frequency range of 12kHz. My question is if this data board would be capable of processing that vibration gathered from the signal and how would I view that data. If there anything else that would need to be purchased or can I just plug this up into a computer or something like that. Is it capable of process the data up to 12kHz?