Hi, I've using CN0510 battery impedance measuring board, and it works fine with correct battery holder.
When I measure the impedance using sweep frequency function (like sweep the frequency from 1 to 10kHz), the result is fine.
But if I test the specific frequency, the impedance is not as precise as using sweep method.
Also, when I using frequency larger then 3kHz, the measurement data is useless, since the RCAL voltage is wrong.
I check AIN1 point at CN0510, the excitation signal is correct as using sweep function.
The console result is like below:
** Set frequency to 3792.68Hz
Hello AD5940-Build Time:20:48:12
This AD594x!
Note: Current Silicon is S2
AD5940LIB Version:v0.2.1
RcalVolt:(2.000000,0.000000)
Fix frequency : 3792.689941
Test condition, AC Vpp: 300.00 mV, DC bias: 3200.00 mV
Freq: 3792.689941 (real, image) = ,0.000000 , -25.000000 ,mOhm
Freq: 3792.689941 (real, image) = ,0.000000 , -25.000000 ,mOhm
Freq: 3792.689941 (real, image) = ,25.000000 , -25.000000 ,mOhm
** Change frequency to 1438.44Hz **
Hello AD5940-Build Time:20:50:42
This AD594x!
Note: Current Silicon is S2
AD5940LIB Version:v0.2.1
RcalVolt:(-37.000000,33.000000)
Fix frequency : 1438.448975
Test condition, AC Vpp: 300.00 mV, DC bias: 3200.00 mV
Freq: 1438.448975 (real, image) = ,11.391376 , -0.650936 ,mOhm
Freq: 1438.448975 (real, image) = ,11.391376 , -0.650936 ,mOhm
Freq: 1438.448975 (real, image) = ,11.391376 , -0.650936 ,mOhm
So, the sweep measurement is good, but single frequency test is failed, I'm wondering why this happened?
I want to test the specific point in EIS so that I can get the optimize frequency faster.
Thanks all of your help!
Have a nice day